• AVR Freaks

Locked[FAQ]So you've found a compiler bug...

Author
JasonK
Moderator
  • Total Posts : 3411
  • Reward points : 0
  • Joined: 2003/11/14 09:49:40
  • Location: Microchip Technology in Arizona, USA
  • Status: offline
2013/07/09 12:47:01 (permalink)
5 (2)

So you've found a compiler bug...

Help us out by reporting it! A good bug report will help us expedite a fix. 

Where should I send the bug report? 
Submit the bug report as a support ticket [http://www.microchip.com/support]. The dedicated support team will get the message and attachments to the people who will investigate, track, and fix the bug. 

What should I put in the bug report? 

  • The version of the compiler. You can get this information by running the compiler with the -v option. 
    .
  • complete input file that will demonstrate the problem. A single statement is (almost) never sufficient. 

    One way to send us a complete example is to attach a pre-processed file. Add -save-temps to your compiler command line and send us the generated preprocessed.i file. Remove extraneous code from the example. 
    .
  • The Build Options (command-line arguments) passed to the compiler, assembler, and linker. If you are building in MPLAB IDE, send us the entire text from the output window following a Build All. 
    .
  • complete description of the behavior that you believe is incorrect. Assume that the bug is not known. What did you expect to happen? What actually happened? For example: When I build with the -Os optimization level, the statement on line 208 of myfile.i assigns 0xFFFF to 16-bit variable foo but I expected it to assign 0x00FF.
Thanks for taking the time to report the issue. The support team at [http://www.microchip.com/support] will do their best to provide you with an effective work around and the Development Tools team will work to address the issue. 
 
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5