• AVR Freaks

MPLABX where I find the HEX file

Author
barbar
Starting Member
  • Total Posts : 34
  • Reward points : 0
  • Joined: 2005/11/21 01:19:27
  • Status: offline
2012/09/06 00:18:19 (permalink)
0

MPLABX where I find the HEX file

In MPLABX after I build the project I can't find the HEX file.
WHere it is place or I need to specifiy same parameters to generat it and where to put it?
#1

1 Reply Related Threads

    DEKTRON
    Super Member
    • Total Posts : 1183
    • Reward points : 0
    • Joined: 2003/11/07 12:35:05
    • Location: Calne, Wiltshire, England
    • Status: offline
    Re:MPLABX where I find the HEX file 2012/09/06 19:46:15 (permalink)
    0
    After you do a production build, the hex file can be found in this folder- 
    (Your Project Folder.x)>dist>default>production
    where "default" is the name of the build configuration set in the project properties (if you don't specify it is called "default")
    Hope it helps -Phil
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5