• AVR Freaks

Hot!PICkitS.dll file for LIN Serial Analyzer

Author
sliu216
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2012/08/24 12:42:01
  • Location: 0
  • Status: offline
2012/08/24 12:44:38 (permalink)
0

PICkitS.dll file for LIN Serial Analyzer

Hello.
I have a question about this .dll file included with the APG LIN Serial Analyzer. Is it possible to use it with C environment to make GUI? I want to use CVI national instruments LabWindow for this. 
post edited by sliu216 - 2012/08/24 14:39:52
#1

1 Reply Related Threads

    ManojSickotra
    New Member
    • Total Posts : 1
    • Reward points : 0
    • Joined: 2019/11/20 15:57:51
    • Location: 0
    • Status: offline
    Re: PICkitS.dll file for LIN Serial Analyzer 2019/11/28 15:08:43 (permalink)
    0
    Hello.
     
    I have recently started using PICkitS.dll to to interface with Microchip APG LIN Serial Analyser. I have managed to initialise the unit and start LIN communication. I think the Transmit funtion is working as I can see Busy Led coming On. Can anyone help me how to use OnReceive or OnAnswer functions. I am trying to capture response back from the target unit.
     
    Thanks
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5