• AVR Freaks

MPLAB X subversion (SVN) 1.7 support

Page: < 12 Showing page 2 of 2
Author
emblocks
Junior Member
  • Total Posts : 74
  • Reward points : 0
  • Joined: 2011/12/22 18:32:24
  • Status: offline
Re:MPLAB X subversion (SVN) 1.7 support 2013/01/08 10:12:32 (permalink)
0
Brian!
It's really a pitty that Microchips announced close collaboration with Netbeans obviously doesn't work as well as it sounds (since MPLAB X is still based on Netbeans 6.9 and the announced Netbeans Support as an independent Plugin seems to be canceled completly) sad...

 
I don't think that  MplabX is still close to the original trunk of Netbeans any more. I guess it's more an embedded fork right now.  
 

Em::Blocks free IDE with PIC18/24/30/32 support
Download is here: www.emblocks.org
#21
prinz3nroll3
Super Member
  • Total Posts : 270
  • Reward points : 0
  • Joined: 2007/03/14 09:38:25
  • Location: germany
  • Status: offline
Re:MPLAB X subversion (SVN) 1.7 support 2013/03/26 09:11:51 (permalink)
+1 (1)
hi,
mplab x 1.70 is the newest version, but the problem still exist, right?
 
we use also svn 1.7.
 
thanks
 
#22
arairan
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2011/03/29 04:39:44
  • Location: 0
  • Status: offline
Re:MPLAB X subversion (SVN) 1.7 support 2013/05/12 20:02:22 (permalink)
+1 (1)
Still not fixed after one year??
#23
fabio.rueda@hotmail.com
New Member
  • Total Posts : 17
  • Reward points : 0
  • Joined: 2012/09/14 18:23:10
  • Location: Santo Andre/Sao Paulo/Brazil
  • Status: offline
Re:MPLAB X subversion (SVN) 1.7 support 2013/05/29 11:11:21 (permalink)
0
I have NOT noted this problem at Mplab X running on MAC OS X.
 
In fact, I dont needed to install any SVN client on the MAC OS X, to MplabX can be able to make the imports, commits and cheouts... maybe Mplab X come with this files to install SVN 1.6.17 automatic that are working on my MAC OS X.
 
Now, in Windows version I had to install SVN Client by my self... and the chosen was the CollabNet Subversion Client 1.7.9 (for Windows 64-bit) that includes all Subversion command-line binaries.
 
And with Windows, yes, I CAN make the "checkout" of the project that was imported to repository before using MAC OS X using Mplab X. BUT, when I try to do a commit using the Windows version the folowing message appears:
 
"it seems that files you are working with were created with an unsupported client version. Please check out your files again with SVN client 1.5.0 or later."
 
There is any difference between MAC OS and Windows OS versions when using MPLAB X ???
 
Why the Mplab X running on MAC OS X doesn't need to install any SVN Client? It already become with the Mplab X install files? If yes, so, what its this version? And more important... why does it work properly and using Windows does NOT ???
post edited by fabio.rueda@hotmail.com - 2013/05/29 18:55:09
#24
janijani
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2013/05/29 10:51:41
  • Location: 0
  • Status: offline
Re:MPLAB X subversion (SVN) 1.7 support 2013/05/29 11:18:32 (permalink)
-2 (2)
sorry, I need to submit irrelevant message.  I just registered.  How do I start a new thread?
#25
DarioG
Allmächtig.
  • Total Posts : 54081
  • Reward points : 0
  • Joined: 2006/02/25 08:58:22
  • Location: Oesterreich
  • Status: offline
Re:MPLAB X subversion (SVN) 1.7 support 2013/05/29 12:04:09 (permalink)
0
janijani

sorry, I need to submit irrelevant message.  I just registered.  How do I start a new thread?

 
New Thread at top of a subforum...

GENOVA :D :D ! GODO
#26
fabio.rueda@hotmail.com
New Member
  • Total Posts : 17
  • Reward points : 0
  • Joined: 2012/09/14 18:23:10
  • Location: Santo Andre/Sao Paulo/Brazil
  • Status: offline
Re:MPLAB X subversion (SVN) 1.7 support 2013/06/03 13:24:45 (permalink)
0
Problem solved (at least for now...)
 
I changed my SVN Client version to 1.6.17... Yes, I do have uninstall the newer version of SVN 1.7 and then look for a older version that are the same used on the MPLABX running on the MACOSX... in other words 1.6.17 version of Subversion Client found in the link below for Windows 32-bit (but running on the Windows 64-bit):
 
First try it: http://sourceforge.net/pr...win32svn/files/1.6.17/
You also can try this one: http://olex.openlogic.com..kages/subversion/1.6.17
 
Now I can make imports, checkout, commits, etc... using MAC OS X MPLAB X 1.80 or Windows MPLAB 1.80 versions...
 
Best regards!!! 
post edited by fabio.rueda@hotmail.com - 2013/06/03 13:27:21
#27
Page: < 12 Showing page 2 of 2
Jump to:
© 2020 APG vNext Commercial Version 4.5