• AVR Freaks

HELP - PICKit 3 Stand Alone Programmer Application v1.0

Author
arktur
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2011/03/13 00:39:11
  • Location: 0
  • Status: offline
2011/03/13 00:57:46 (permalink)
0

HELP - PICKit 3 Stand Alone Programmer Application v1.0


I installer an environment under PICkit-3 " PICkit 3 Stand Alone Programmer App V1.0 Windows ".
" PICkit 3 Stand Alone Programmer App V1.0 Windows " is opened, but at attempt to begin to work the message emerges, that can not find a file "PK3RS_011304.hex" and on it all stops.
What is this file and where it(him) to take? For what he is necessary?

Attached Image(s)

#1

3 Replies Related Threads

    trevor
    Super Member
    • Total Posts : 575
    • Reward points : 0
    • Joined: 2010/05/05 21:02:18
    • Location: The LAN Downunder
    • Status: offline
    Re:HELP - PICKit 3 Stand Alone Programmer Application v1.0 2011/03/13 04:20:57 (permalink)
    0
    Did you read the "Release Notes for the PICkit 3 Programmer Application" ?

    I think it describes your problem and how to fix it.
    
                    
                    
                
    #2
    arktur
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2011/03/13 00:39:11
    • Location: 0
    • Status: offline
    Re:HELP - PICKit 3 Stand Alone Programmer Application v1.0 2011/03/14 22:18:35 (permalink)
    0

    I have two versions MPLAB IDE: V8.50 and V8.63.
    Really there there are similar files:

    In the version V8.50 - PK3RS_011101.hex
    In the version V8.63 - PK3RS_011400.hex

    And this PICkit 3 requests a file PK3RS_011304.hex
    On logic it is possible, what the required file can be in an environment MPLAB IDE any of the versions above V8.50, but is lower V8.63?
    I tried to find this file on a site MIKROCHIP - but while without result.
    If someone has a file PK3RS_011304.hex - inform!
    #3
    jnherm
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2009/09/12 08:21:54
    • Location: 0
    • Status: offline
    Re:HELP - PICKit 3 Stand Alone Programmer Application v1.0 2011/03/14 22:28:22 (permalink)
    0
    PICKit 3 Stand Alone Programmer Application v1.0 sucks! Just wait for the next version.... I have the same problem...
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5