• AVR Freaks

LockedProgramming issue with 18F46K22 family of devices

Author
H H
Administrator
  • Total Posts : 1197
  • Reward points : 0
  • Joined: 2003/11/07 00:00:00
  • Status: offline
2011/01/24 16:09:58 (permalink)
0

Programming issue with 18F46K22 family of devices

Tools:  ICD3/REAL ICE/PICkit 3
Device: 18F46K22 family
Version affected:  MPLAB IDE v8.63
 
We have found a programming issue affecting the 18FxxK22 family of devices.  During programming of the device in the debug mode, you will see this:
 
The following memory regions failed to program correctly:
Debug Executive
Programming failed
 
A patch can be found here:  www.microchip.com\IDE 
Place MASTERDB.MCC in the C:\Program Files\Microchip\MPLAB IDE\Device directory
Place the RIDE_04_BANK99_010303 in the C:\Program Files\Microchip\MPLAB IDE\REAL ICE directory.
 
If using PICkit 3, place RIDE_04_BANK99_010303 in C:\Program Files\Microchip\MPLAB IDE\PICkit 3
 
The fix will be incorporated into the MPLAB IDE v8.66 build scheduled for our February release.  Sorry for the inconvenience this has caused.
 
 
post edited by H H - 2011/01/24 16:11:25
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5