• AVR Freaks

MCP2200 parity problem

Author
pedja089
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2010/04/23 12:50:54
  • Location: 0
  • Status: offline
2010/11/13 15:31:38 (permalink)
0

MCP2200 parity problem

How to set up even parity on MCP2200?
When I configure port to 2400,E,8,1 in software, parity bit isn't sent. But when receiving data with parity, it receive correctly.
#1

2 Replies Related Threads

    t.szanto
    New Member
    • Total Posts : 1
    • Reward points : 0
    • Joined: 2011/03/18 08:00:13
    • Location: 0
    • Status: offline
    Re:MCP2200 parity problem 2011/03/18 08:01:55 (permalink)
    0
    Hello,

    I have the same problem now. Do you know the solution?

    Thanks
    #2
    icserny
    Super Member
    • Total Posts : 258
    • Reward points : 0
    • Joined: 2008/09/07 13:27:08
    • Location: Debrecen, Hungary
    • Status: offline
    Re:MCP2200 parity problem 2011/03/18 11:06:01 (permalink)
    0
    The Datasheet says: "The MCP2200 responds by setting the baud rate only. The other parameters (Data Bits, Parity, Stop Bits) remain unchanged." This means that only mode 8,N,1 can be used. :-(
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5