• AVR Freaks

PICkit 2 support Please!

Author
smartin
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2010/10/28 16:50:29
  • Location: 0
  • Status: offline
2010/11/04 17:22:27 (permalink)
0

PICkit 2 support Please!

It's unfortunate that support for the PICkit2 was not included. Will it also not be in the final product?
#1

7 Replies Related Threads

    amos1969
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2009/10/25 15:32:24
    • Location: Bolton
    • Status: offline
    Re:PICkit 2 support Please! 2010/11/05 03:48:40 (permalink)
    0
    Seconded.

    (I'd go with a PICkit 3 but I use Linux and it doesn't appear to be natively supported)
    #2
    dpc
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2003/11/07 12:36:28
    • Status: offline
    Re:PICkit 2 support Please! 2010/11/19 11:14:13 (permalink)
    0
    Microchip does intend to provide PICkit 2 support in MPLAB X.
    #3
    pauljclarke
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2009/11/06 07:29:29
    • Location: 0
    • Status: offline
    Re:PICkit 2 support Please! 2010/11/20 06:54:09 (permalink)
    0
    dpc

    Microchip does intend to provide PICkit 2 support in MPLAB X.


    At the Microchip EDF last week they are saying that they do not see PICKit2 being added at any time for MPLAB'X

    Disappointing.!
    #4
    DaytonaFiend
    Administrator
    • Total Posts : 138
    • Reward points : 0
    • Joined: 2007/11/10 10:54:30
    • Location: Microchip Technology
    • Status: offline
    Re:PICkit 2 support Please! 2010/11/21 11:35:01 (permalink)
    0
    Hi all,
       PICKit2 MOST DEFINITELY WILL BE SUPPORTED. It is not available in Beta4 but hopefully should be ready for the full release early next year (it may follow a little bit later). The programmers in development systems are doing a brilliant job with MPLAB X and they just have to prioritize the work.


    ..DF

    p.s. the problem with these semiars is that one presenters has to remember an awful lot of information for one day!! Smile and may not get the information over exactly right.

    #5
    Stefan Uhlemayr
    Super Member
    • Total Posts : 4292
    • Reward points : 0
    • Joined: 2005/05/12 12:25:46
    • Location: Germany
    • Status: offline
    Re:PICkit 2 support Please! 2010/11/21 11:39:32 (permalink)
    0
    DaytonaFiend

    Hi all,
       PICKit2 MOST DEFINITELY WILL BE SUPPORTED. ...
    Very good news! Smile
    #6
    vaclavpe
    Starting Member
    • Total Posts : 66
    • Reward points : 0
    • Joined: 2007/07/23 13:28:30
    • Location: 0
    • Status: offline
    Re:PICkit 2 support Please! 2010/11/25 04:44:55 (permalink)
    0
    pauljclarke

    At the Microchip EDF last week they are saying that they do not see PICKit2 being added at any time for MPLAB'X

    Disappointing.!

    Very disappointing. I used PICs for 8 years and lack of debugging on Linux (my primary OS) and SRAM were reasons to move to Cortex M3 when project was bigger. It seems to me that Cortex M0 will be more suitable for something smaller. People accustomed to good things like debugging very quickly.

    As I see, my PicKit2 (used for programming only) stays in my drawer...

    #7
    genesis31
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2010/11/09 03:33:52
    • Location: 0
    • Status: offline
    Re:PICkit 2 support Please! 2010/11/25 11:57:04 (permalink)
    0
    Given the popularity of the PICkit 2 (at least from what I see) I would have assumed it would have been given a slightly higher priority even if it is not at the high end of the hardware scale. However I am delighted to learn that it will find its way into MPLAB X.
    #8
    Jump to:
    © 2020 APG vNext Commercial Version 4.5