RE: Programming dsPIC30F2010 with MPLAB ICD 2
2006/04/15 14:21:51
(permalink)
Thank you for this thread!
I am just happy to see I didn't blow up my dsPIC due to my interfacing or <?programming?>. The ICD2 initially recognized the dSPIC30F2010, but after a couple debug cycles displayed the "Invalid target device ID error."
1) Can any harm be done to the dSPIC30F2010 by repeatedly attempting to communicate with an older ICD2 (I know, the definition of insanity... mine is a rev. 15)
2) If one does the mods outlined here, will there be any issues with communicating with other PICS? I also use the 18F452.
Is there a recommended modification that will work with both, preferibly without jumpers?
Thanks for the tips!
Friedrich Kirk