DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
PLACEHOLDER FOR Code Module Library
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
Code for sending int/floats as raw binary data (chars) to USART
2007/11/16 08:19:57
(permalink)
char i,*p; float f; // same goes for int or alike p=(char *)&f; for(i=0; i<sizeof(float); i++) { putcUSART(*p++); } Keep in mind that this value, i.e. the sequence of bytes sent, is "Machine Dependant" (i.e. little endian/big endian sensitive) so the other end of the communication must agree on that.
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
USB WAV Player (with schematic and code)
2007/11/16 15:34:41
(permalink)
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
FAT16 (Memory Disk Drive File System Library)
2007/11/16 15:36:40
(permalink)
Hi, Microchip released the first version of their Memory Disk Drive File System Library. It's compatible with FAT16. You can find the documentation and the source files on Microchip website, application note AN1045. I tested the source and sample files with my older hardware design (compact flash card, with bit-transaction), with success. This is exactly what I've been looking and waiting for..... Thx to Microchip della
post edited by DarioG - 2007/11/16 15:40:32
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
sprintf() using float, for C18
2007/11/16 15:37:28
(permalink)
char buf[8]; sprintf(buf,"%d.%02u", (int)f , ((int) (((f)-(int)f) * 100)) ); You can choose how many figures you wish, changing the "02u" and "*100" accordingly, and the "buf" size. ADDED by Ren: All of the other limitations aside, I tried this method and noticed that it fails to handle negative numbers. Adding fabs() to the calculation for the decimal part solves that issue, and only added 3 bytes to the program. sprintf(buf,"%d.%02u", (int) d, (int) fabs(((d - (int) d ) * 100))); ADDED by 1and0 for handling of the -1..0 range ( http://www.microchip.com/...7&mpage=1#699128): void ftoa(float value, char *string) { if (value < 0) { *string++ = '-'; value = -value; } sprintf(string, (const far rom char *) "%lu.%03u", (long) value, (int) ((value - (long) value) * 1000. + 0.5)); } also this one: http://support2.microchip....aspx?ID=SQ6UJ9A003PQX
post edited by DarioG - 2013/01/12 02:42:32
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
A Class to do RS232 (Serial Port) Communications in C++ in Windows
2007/11/16 15:38:46
(permalink)
Attached code (rename it to ".ZIP") PS: Usage example: //begin myComm=new CSerCommObject(comPortString); // such as "COM1:9600,N,8,1 myComm->Open(); //use if(i=myComm->Send((BYTE *)"test",4)) { // do something } char myBuf[16]; if(i=myComm->Receive((BYTE*)myBuf,8,2000)) { // 2secs time allowed forreceive // do something } //end myComm->Close(); delete myComm; Attachment (1)
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
Software I2C routines for PIC18F
2007/11/16 15:42:40
(permalink)
/************************************************************** Start Bit Subroutine this routine generates a start bit (Low going data line while clock is high) **************************************************************/ void I2CSTART(void) { // SWStartI2C(); m_I2CClkBit=0; // make sure clock is low m_I2CDataBit=1; // make sure data is high I2CDataTris=0; // set data and clock lines for output I2CDelay(); setClockHigh(); // CLK=1 I2CDelay(); m_I2CDataBit=0; // data line goes low during high clock for start bit I2CDelay(); m_I2CClkBit=0; // start clock train I2CDelay(); } /************************************************************ Stop Bit Subroutine This routine generates a stop bit (High going data line while clock is high) ************************************************************/ void I2CSTOP(void) { // SWStopI2C(); m_I2CDataBit=0; // make sure data line is low m_I2CClkBit=0; // make sure clock is low I2CDataTris=0; // set data/clock lines as outputs m_I2CClkBit=1; // set clock high I2CDelay(); m_I2CDataBit=1; // data goes high while clock high for stop bit I2CDelay(); m_I2CClkBit=0; // set clock low again I2CDelay(); I2CDataTris=1; // set data line as input // m_I2CClkBit=1; // set clock idle setClockHigh(); // CLK=1 // questa e' un'altra attesa, per i dispos. (tipo PICBELL, PICWDI2C) che il WAIT lo fanno DOPO lo STOP! // m_I2CClkBit=0; I2CDelay(); } /************************************************************* BITOUT routine takes the bit of data in C and transmits it to the serial EE device *************************************************************/ void I2CBITOUT(byte n) { I2CDataTris=0; // set data,clock as outputs if(n) // check for state of data bit to xmit m_I2CDataBit=1; // output a low bit else m_I2CDataBit=0; // high? set data line high Nop(); // dev'esserci un min. ritardo tra il cambio in DATA e la salita di CLK Nop(); m_I2CClkBit=1; // set clock line high I2CDelay(); m_I2CClkBit=0; // return clock line low I2CDelay(); // retlw 0 } /************************************************************** BITIN routine reads one bit of data from the serial EE device and stores it in C **************************************************************/ byte I2CBITIN(void) { /*overlay*/ byte i; I2CDataTris=1; // make sdata an input line I2CDelay(); m_I2CClkBit=1; // set clock line high I2CDelay(); // just sit here a sec i = m_I2CDataBit ? 1 : 0; // read the data bit m_I2CClkBit=0; // set clock line low return i; } void setClockHigh(void) { // Gestisce WAIT_STATE dello slave (CLK basso)... che puo' succedere SEMPRE! m_I2CClkBit=1; I2CClkTris=1; // CLK e' input I2CDelay(); do { ClrWdt(); } while(!m_I2CClkBit); I2CClkTris=0; // CLK e' output } /**************************************************************** Transmit Data Subroutine This routine takes the byte of data stored in the 'temp' register and transmits it to the serial EE device. It will then send 1 more clock to the serial EE for the acknowledge bit. If the ack bit from the part was low then the transmission was sucessful. If it is high, then the device did not send a proper ack bit and the ack fail LED will be turned on. ****************************************************************/ #define I2CTXSlaveAddrW() I2CTXByte(0xA0) #define I2CTXSlaveAddrR() I2CTXByte(0xA1) byte I2CTXByte(byte n) { /*overlay*/ static byte I2CData,I2CCnt; I2CData=n; for(I2CCnt=0; I2CCnt<8; I2CCnt++) { // set the #bits to 8 I2CBITOUT(I2CData & 0x80); // send the bit to serial EE I2CData <<= 1; // rotate I2CData/txbuf left, bit in CARRY } // 8 bits done? // no - go again // read ack bit I2CDataTris=1; I2CDelay(); setClockHigh(); // aspetto ACK // Per WAIT_STATE dello slave (CLK basso)... NON e' chiaro se PRIMA o DOPO ACK... (PicBell lo fa dopo!) // questo lo controlla SEMPRE! I2CDelay(); // dopo Delay, qua arrivo con W=0 e Z=1 I2CCnt=m_I2CDataBit; // Z=1 se ACK=OK (basso), altrimenti Z=0 e W!=0 m_I2CClkBit=0; if(I2CCnt) { // check ack bit m_MemCardLedBit=1; // spegne! set acknowledge fail LED if the device did not pull data low return 0; // 0=ERR } return 1; // 1=OK } /**************************************************************** Receive data routine This routine reads one byte of data from the part into the 'I2CData' register. ****************************************************************/ byte I2CRXByte(void) { static /*overlay*/ byte I2CData,I2CCnt; // SWReadI2C(); // I2CData=0; // clear input buffer non serve! for(I2CCnt=0; I2CCnt<8; I2CCnt++) { // set the #bits to 8 I2CData <<= 1; // rotate I2CData 1 bit left I2CData |= I2CBITIN(); // read a bit // STATUSbits.C = 1; // la presenza di ASM disabilita l'ottimizzazione, quindi PEGGIORA! // Rlcf(input); // Rotate the carry into the data byte } // 8 bits done? // no, do another return I2CData; } /**************************************************************** Receive data routine This routine reads one byte of data from the part into the 'I2CData' register. It then sends a high ACK bit to indicate that no more data is to be read ****************************************************************/ byte I2CRX1Byte(void) { static /*overlay*/ byte I2CData,I2CCnt; // I2CData=0; // clear input buffer non serve! for(I2CCnt=0; I2CCnt<8; I2CCnt++) { // set the #bits to 8 // STATUSbits.C = 1; // la presenza di ASM disabilita l'ottimizzazione, quindi PEGGIORA! // Rlcf(input); // Rotate the carry into the data byte I2CData <<= 1; // rotate I2CData 1 bit left I2CData |= I2CBITIN(); // read a bit } // 8 bits done? // no, do another // set ack bit = 1 I2CBITOUT(1); // to finish transmission return I2CData; } /************************************************************** READ (read routine) This routine reads 8 consecutive addresses of the serial EE device starting at address 00 in the random access mode (non-sequential read). Reading the device using the random access mode requires that the address pointer be set for every byte before the read takes place. The address pointer is set by sending a 'write mode' control byte with the address of the location to read. ***************************************************************/ byte I2CReadRandom(byte n) { static /*overlay*/ byte I2CData; // bcf port_a,ackf ; clear the ack fail LED if on I2CSTART(); // generate start bit // // now send the write control byte and // address to set the pointer // I2CTXSlaveAddrW(); // get slave address and write mode // movfw I2CAddr ; get word address I2CTXByte(n); // and send it // now read one byte from the part I2CSTART(); // generate start bit I2CTXSlaveAddrR(); // get slave address and read mode I2CData=I2CRX1Byte(); // read 1 byte from serial EE I2CSTOP(); // send stop bit to end transmission return I2CData; } byte I2CReadRandom16(word n) { byte I2CData; // bcf port_a,ackf ; clear the ack fail LED if on I2CSTART(); // generate start bit // // now send the write control byte and // address to set the pointer // I2CTXSlaveAddrW(); // get slave address and write mode // move word address (HIGH) I2CTXByte(*(((byte *)&n)+1)); // and send it // move word address (LOW) I2CTXByte(*((byte *)(&n))); // and send it // now read one byte from the part I2CSTART(); // generate start bit I2CTXSlaveAddrR(); // get slave address and read mode I2CData=I2CRX1Byte(); // read 1 byte from serial EE I2CSTOP(); // send stop bit to end transmission return I2CData; } /************************************************************** READ (sequential read routine) This routine reads 8 consecutive addresses of the serial EE device starting at address 00 in the sequential read mode. Reading in this mode is more efficient than the random read mode as the control byte and address have to be sent only once at the beginning of the sequence. As many consecutive addresses as needed can then be read from the part until a stop bit is sent. In the read mode, the PIC 16C54 must send the acknowledge bit after every 8 data bits from the device. When the last byte needed has been read, then the controller will send a high acknowledge bit and then a stop bit to halt transmission from the device. ***************************************************************/ byte I2CRead8Seq(byte n,byte I2CCntB) { // entra W=indirizzo part. lettura, FSR punta al buffer static /*overlay*/ byte *p; // bcf port_a,ackf ; clear the ack fail LED if on p=I2CBuffer; // bank1, ISP=0! I2CSTART(); // generate start bit I2CTXSlaveAddrW(); // send slave address and write mode // get word address I2CTXByte(n); // and send it I2CSTART(); // generate start bit I2CTXSlaveAddrR(); // send slave address and read mode I2CRead8Seq2: *p++=I2CRXByte(); // read 1 byte from device if(!--I2CCntB) { // are all 8 bytes read? // no, send low ack and do another // yes, send high ack bit I2CBITOUT(1); // to stop tranxmission I2CSTOP(); // and send a stop bit return 8; } // send low ack bit I2CBITOUT(0); // to continue transmission goto I2CRead8Seq2; //and read another byte } /************************************************************** READ16 (sequential read routine) This routine reads 8 consecutive addresses of the serial EE device starting at given 16bit address in the sequential read mode. Reading in this mode is more efficient than the random read mode as the control byte and address have to be sent only once at the beginning of the sequence. As many consecutive addresses as needed can then be read from the part until a stop bit is sent. In the read mode, the PIC 16C54 must send the acknowledge bit after every 8 data bits from the device. When the last byte needed has been read, then the controller will send a high acknowledge bit and then a stop bit to halt transmission from the device. ***************************************************************/ byte I2CRead16Seq(word n,byte I2CCntB) { // entra indirizzo part. lettura, FSR punta al buffer static /*overlay*/ byte *p; // bcf port_a,ackf ; clear the ack fail LED if on I2CSTART(); // generate start bit I2CTXSlaveAddrW(); // send slave address and write mode // move word address (HIGH) I2CTXByte(*(((byte *)&n)+1)); // and send it // move word address (LOW) I2CTXByte(*((byte *)(&n))); // and send it I2CSTART(); // generate start bit I2CTXSlaveAddrR(); // send slave address and read mode p=I2CBuffer; I2CRead16Seq2: *p++=I2CRXByte(); // read 1 byte from device if(!--I2CCntB) { // are all n bytes read? // no, send low ack and do another // yes, send high ack bit I2CBITOUT(1); // to stop tranxmission I2CSTOP(); // and send a stop bit return 16; } // send low ack bit I2CBITOUT(0); // to continue transmission goto I2CRead16Seq2; // and read another byte } byte I2CReadRTC(byte I2CCntB) { // entra num. byte da leggere, buffer static /*overlay*/ byte *p; // bcf port_a,ackf ; clear the ack fail LED if on p=I2CBuffer; // bank1, ISP=0! I2CSTART(); // generate start bit I2CTXByte(0xD0); // DS1337C // send slave address and read mode I2CTXByte(0); // send register address I2CSTART(); // generate start bit I2CTXByte(0xD1); // DS1337C I2CRead8Seq2: *p++=I2CRXByte(); // read 1 byte from device if(!--I2CCntB) { // are all 8 bytes read? // no, send low ack and do another // yes, send high ack bit I2CBITOUT(1); // to stop tranxmission I2CSTOP(); // and send a stop bit return 1; } // send low ack bit I2CBITOUT(0); // to continue transmission goto I2CRead8Seq2; //and read another byte } /**************************************************************** Byte Write Routine This routine writes the data in "temp" to 8 consecutive bytes in the serial EE device starting at address 00. This routine waits 10mS after every byte to give the device time to do the write. This program repeats forever. *****************************************************************/ void I2CWriteByte(byte n, byte b) { static /*overlay*/ byte I2CAddr,I2CCnt; // SWWriteI2C(); // clrf port_a ; clear all LEDs I2CAddr=n; // set starting address to W // temp=0x55; // set data to write as 55h // set number of bytes for(I2CCnt=0; I2CCnt<8; I2CCnt++) { // set the #bits to 8 I2CSTART(); // generate start bit I2CTXSlaveAddrW(); // send slave address and write mode // move word address I2CTXByte(I2CAddr); // and send it I2CTXByte(b); // move data byte and transmit it I2CSTOP(); // generate stop bit // movlw 10 // movwf loops ; set delay time to give // call WAIT ; 10 ms wait after every byte I2CWritePagePoll(); I2CAddr++; // add 1 to address counter } // all 8 bytes written? // no, do another byte } /**************************************************************** Page Write Routine This routine uses page mode to write the data in "temp" to 8 consecutive bytes in the serial EE device starting at address 00. This routine waits 10mS after every page to give the device time to do the write. This routine executes forever *****************************************************************/ void I2CWritePage(byte n,byte I2CCntB) { // entra W=indirizzo part. lettura, (FSR usato per buffer) static /*overlay*/ byte *p; // clrf port_a ; clear all LEDs p=I2CBuffer; I2CSTART(); // generate start bit I2CTXSlaveAddrW(); // send slave address and write mode // move word address I2CTXByte(n); // and send it do { I2CTXByte(*p++); // and transmit it } while(--I2CCntB); // all n bytes written? // no, do another I2CSTOP(); // yes,generate stop bit // movlw 10 // movwf loops ; set delay time to give // call WAIT ; 10 ms wait after every byte Delay_mS(20); // 50mS } void I2CWriteRTC(byte n,byte I2CCntB) { // entra W=indirizzo part. lettura, (FSR usato per buffer) static /*overlay*/ byte *p; // clrf port_a ; clear all LEDs p=I2CBuffer; I2CSTART(); // generate start bit // send slave address and write mode I2CTXByte(0xD0); // DS1337C // move register address I2CTXByte(n); // and send it do { I2CTXByte(*p++); // and transmit it } while(--I2CCntB); // all n bytes written? // no, do another I2CSTOP(); // yes,generate stop bit // movlw 10 // movwf loops ; set delay time to give // call WAIT ; 10 ms wait after every byte } /**************************************************************** Page Write 16 Routine (8 bytes, address a 16 bit) This routine uses page mode to write the data in "temp" to 8 consecutive bytes in the serial EE device starting at given address . This routine waits 10mS after every page to give the device time to do the write. This routine executes forever *****************************************************************/ #define I2CWritePage16Default() I2CWritePage16((word)&I2CAddr) byte I2CWritePage16(word n,byte I2CCntB) { // entra W=puntat. all'indirizzo part. lettura, (FSR usato per buffer) static /*overlay*/ byte *p; // clrf port_a ; clear all LEDs I2CSTART(); // generate start bit I2CTXSlaveAddrW(); // send slave address and write mode // move word address (HIGH) I2CTXByte(*(((byte *)&n)+1)); // and send it // move word address (LOW) I2CTXByte(*((byte *)(&n))); // and send it p=I2CBuffer; do { I2CTXByte(*p++); // and transmit it } while(--I2CCntB); // move data byte // all n bytes written? // no, do another I2CSTOP(); // yes,generate stop bit // movlw 10 // movwf loops ; set delay time to give // call WAIT ; 10 ms wait after every byte Delay_mS(20); // 20mS return 16; } byte I2CWritePagePoll(void) { byte I2Cpollcnt,i; I2Cpollcnt=100; // set max number of times to poll as 100 do { I2CSTART(); // generate start bit i=I2CTXSlaveAddrW(); // send slave address and write mode if(i) // was the ack bit low? goto exitpoll; // yes, do another byte } while(--I2Cpollcnt); // is poll counter down to zero? // no, poll again. Otherwise the part is // bsf port_a,timeout ; not responding in time so set timeout LED and continue on exitpoll: ; } void I2CDelay(void) { // circa 2,5uSec (400KHz operation) /*overlay*/ static byte uSec; // 1.25 ca. uSec=1; do { ClrWdt(); // Clear the WDT Delay1TCY(); // TARARE!! @48MHz?? Delay1TCY(); Delay1TCY(); // Delay1TCY(); } while(--uSec); } (unfortunately this can't be retrieved from cache... will try reposting it.)
post edited by DarioG - 2007/12/04 01:59:10
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
Working CONFIG settings for 18F2550/4550
2007/11/17 06:56:55
(permalink)
#pragma config WDT = OFF, WDTPS = 1024, MCLRE=ON, STVREN=ON, LVP=OFF // either watchdog disabled... //#pragma config WDT = ON, WDTPS = 1024, MCLRE=ON, STVREN=ON, LVP=OFF // ..or watchdog enabled #pragma config PLLDIV=2, CPUDIV=OSC1_PLL2, USBDIV=2, FOSC=HSPLL_HS, IESO=OFF, PWRT=OFF, BOR=ON, BORV=2 // 8MHz Crystal, 48MHz Core, 48MHz SIE engine (USB2, full speed) #ifndef __EXTENDED18__ #pragma config VREGEN=ON, LPT1OSC=OFF, PBADEN=OFF, CCP2MX=ON, XINST=OFF, DEBUG=OFF // for Extended Mode... #else #pragma config VREGEN=ON, LPT1OSC=OFF, PBADEN=OFF, CCP2MX=ON, XINST=ON, DEBUG=OFF // ...or normal Mode #endif ADD: also take a look at http://users.edpnet.be/rosseel01/DRO/PIC/18F2455_2550_4455_4550_Usb_Clock.htm
post edited by DarioG - 2008/11/25 14:16:22
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
TEMPLATE for interrupts on 18F parts with C18
2007/11/21 02:58:11
(permalink)
/** I N T E R R U P T V E C T O R S *****************************************/ #pragma code high_vector=0x08 #define SILICON_REV_A3 void interrupt_at_high_vector(void) { _asm #ifdef SILICON_REV_A3 CALL Foo, 1 // store current value of WREG,BSR, STATUS for a second time RETFIE 1 // FAST Foo: POP // clears return address of Foo call goto high_isr #else goto high_isr #endif _endasm } #pragma code #pragma code low_vector=0x18 void interrupt_at_low_vector(void) { _asm goto low_isr _endasm } #pragma code /** D E C L A R A T I O N S **************************************************/ /****************************************************************************** * Function: void high_isr(void) * PreCondition: None * Input: * Output: * Side Effects: * Overview: *****************************************************************************/ #pragma interrupt high_isr // nosave=section("MATH_DATA"),section(".tmpdata") // OPTIONAL void high_isr(void) { if(INTCONbits.TMR0IF) { // Timer 0.. EXAMPLE INTCONbits.TMR0IF=0; // clear bitIRQ } } /****************************************************************************** * Function: void low_isr(void) * PreCondition: None * Input: * Output: * Side Effects: * Overview: *****************************************************************************/ #pragma interruptlow low_isr //nosave=section("MATH_DATA"),section(".tmpdata") //OPTIONAL void low_isr(void) { } #pragma code
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
Several ways to calculate parity
2007/11/24 13:09:06
(permalink)
// calcola la parita': entra W, esce 0 se E e 1 se O BOOL GetParita(byte n) { static byte p; #ifdef DARIO p=n >> 1; // Microchip AN774 p ^= n; n= p >> 2; p ^= n; n= p >> 4; p ^= n; return (p & 1); #endif #ifdef OLDPARITA if(n & 0x1) p++; if(n & 0x2) p++; if(n & 0x4) p++; if(n & 0x8) p++; if(n & 0x10) p++; if(n & 0x20) p++; if(n & 0x40) p++; if(n & 0x80) p++; #endif //From: John Payson //comments from Andrew Warren of Fast Forward Engineering //8-bit parity //This routine will leave the parity of X in X.0 // while blenderizing most of the rest of X p=n; _asm movlb p swapf p, 0, 1 //x= abcdefgh w = efghabcd xorwf p, 1, 1 //x= abcdefgh w = efghabcd // xor efghabcd rrncf p, 0, 1 //x= abcdefgh w = -abcdefg // xor efghabcd xor -efghabc xorwf p, 1, 1 //x= abcdefgh w = -abcdefg // xor efghabcd xor -efghabc // xor -abcdefg // xor -efghabc // at this point, the parity for half the bits // (a, b, e, and f) is in bit 2 of X, and the // parity for the other half (bits c, d, g, and h) // is in bit 0 of X. btfsc p, 2, 1 // if the parity of (a,b,e,f) is 0, // then the parity of (a,b,c,d,e,f,g,h) // is equal to the parity of (c,d,g,h)... // which is already in bit 0, so skip ahead. incf p, 1, 1 // otherwise, the parity of (a,b,e,f) is 1, // so the parity of (a,b,c,d,e,f,g,h) is // NOT equal to the parity of (c,d,g,h). // invert bit 0. // at this point, bit 0 contains the parity of // (a,b,c,d,e,f,g,h). _endasm #ifdef RIC CheckParity: swapf X, w ; John's idea: reducing byte to nibble xorwf X, w addlw 41H ; bit 1 becomes B0^B1 and bit 7 becomes B6^B7 iorlw 7CH ; for carry propagation from bit 1 to bit 7 addlw 2 ; Done! the parity bit is bit 7 of W andlw 80H ; set NZ if odd parity, and leave 00 or 80 in W return #endif #define PARITY(b) ((((((b)^(((b)<<4)|((b)>>4))) + 0x41) | 0x7C ) +2 ) & 0x80) return p & 1; } See also: http://graphics.stanford....hacks.html#ParityNaive
post edited by DarioG - 2013/05/20 03:16:35
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
Write/Read to/from EEprom in C18
2007/12/04 01:56:05
(permalink)
// ------------------------------------------------------------------------------------- void EEscrivi_(SHORTPTR addr,byte n) { EEADR = (byte)addr; EEDATA=n; EECON1bits.EEPGD=0; // Point to Data Memory EECON1bits.CFGS=0; // Access EEPROM EECON1bits.WREN=1; // INTCONbits.GIE = 0; // disattiva interrupt globali... e USB? EECON2=0x55; // Write 55h EECON2=0xAA; // Write AAh EECON1bits.WR=1; // abilita write. do { ClrWdt(); } while(EECON1bits.WR); // occupato ? // INTCONbits.GIE = 1; // attiva interrupt globali EECON1bits.WREN=0; // disabilita write. } byte EEleggi(SHORTPTR addr) { EEADR=(byte)addr; // Address to read EECON1bits.EEPGD=0; // Point to Data Memory EECON1bits.CFGS=0; // Access EEPROM EECON1bits.RD=1; // EE Read return EEDATA; // W = EEDATA } SHORTPTR is actually an unsigned char, in this implementation. Typedef'd for future extensions.
|
corvette321
Super Member
- Total Posts : 727
- Reward points : 0
- Joined: 2006/10/31 19:17:07
- Location: Florida
- Status: offline
working circular buffer
2007/12/13 09:37:22
(permalink)
guys here is my finished and tested circular buffa code if anyone wants it!!! feel free to copy it. this one is well suited for USART becuase it works with null terminated strings... and returns a null if empty... this one handles empty and full also. unsigned int head, tail = 0; unsigned int length = 127; unsigned char buffer_full=0; unsigned char buffer_empty=1; char rcv_buffa[128]; //write a byte to receive buffa //this process assumes tail is always an empty spot //if tail=head then empty , if (tail= head -1) then full // void write_rcvbuffa(unsigned char blah123) { //check for a full buffer if ((buffer_full) | ((tail+1)==head) | ((tail==length) & (head==0))) { xbee_rts=1; //inhibit unit from sending more data buffer_full=1; } //if buffer not full else { //write the byte and inc to next empty slot rcv_buffa[tail] = blah123; if (tail >= length) { tail = 0; } else { tail++; } //update flags buffer_empty=0; if (((tail+1)==head) | ((tail==length) & (head==0))) { buffer_full=1; xbee_rts=1; //inhibit more stuff from comming until buffer is not empty } } } //end write a byte to receive buffa // read a byte from receive buffer unsigned char read_rcvbuffa(void) { //return a null if buffer is empty, otherwise read 1 from head and increment // then returns the value at head. // then examines if buffer is empty and sets flag as appropriate for next read (or write) if ((buffer_empty) | (head==tail)) { Data1=0x00; //null value xbee_rts=0; //good to go buffer_empty=1; } else { //read 1 from head and inc head Data1 = rcv_buffa[head]; if (head >= length) { head = 0; } else { head++; } //update flags buffer_full=0; xbee_rts=0; if (head==tail) { buffer_empty=1; xbee_rts=0; //good to go } } return Data1; } // end read byte from receive buffa lemme know if anyone needs additional info or help with it :) this one is tested with xbee pro module as a receive buffer. im gonna use it for a transmit one too i think. the RTS control stuff can be deleted if your not using it... (or not using an xbee module hahah)
post edited by corvette321 - 2007/12/13 09:44:51
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
1-wire Dallas code in Assembler for 16F PICs
2008/01/06 05:54:12
(permalink)
; BEGINNING OF CODE btfsc PORTB,SPI_232_I ; se e' basso, c'e' iButton! goto noIButton movlw TO_ADDR movwf DstAddr movlw 55 ; notifica da iButton call SetFrame movlw 250 EXTENDED_CALL Delay_uS ; aspetto 250uSec movlw 0x33 ; comando READ-ROM EXTENDED_CALL DoDallasOut bcf PORTB,SPI_232_I ; DATA=0 movlw 8 ; 8 byte... movwf temp3 movlw BuffO6Arg ; ...a partire da parm1 del pacch. in uscita movwf FSR _iButton: EXTENDED_CALL DoDallasIn MY_PAGESEL _iButton movwf INDF incf FSR,f decfsz temp3,f goto _iButton noIButton: ; END... ; SUPPORT ROUTINES DoDallasOut: ; entra W= valore; tSlot=100uS movwf temp movlw 8 movwf tempC call setDataOutput DoDallasOut1: bcf PORTB,SPI_232_I movlw 90 btfsc temp,0 movlw 10 call Delay_uS bsf PORTB,SPI_232_I rrf temp,f movlw 10 btfsc STATUS,C movlw 90 call Delay_uS decfsz tempC,f goto DoDallasOut1 return DoDallasIn: ; esce W= valore; tSlot=100uS movlw 8 movwf tempC DoDallasIn1: call setDataOutput movlw 5 call Delay_uS call setDataInput movlw 10 call Delay_uS bcf STATUS,C btfsc PORTB,SPI_232_I bsf STATUS,C rrf temp,f movlw 85 call Delay_uS decfsz tempC,f goto DoDallasIn1 movfw temp return setDataOutput: bsf STATUS,RP0 ; Bank 1 bcf TRISB,SPI_232_I ; DATA e' output bcf STATUS,RP0 ; Bank 0 return setDataInput: bsf STATUS,RP0 ; Bank 1 bsf TRISB,SPI_232_I ; DATA e' input bcf STATUS,RP0 ; Bank 0 return
|
ren
Super Member
- Total Posts : 654
- Reward points : 0
- Joined: 2006/04/20 16:17:49
- Location: So Cali
- Status: offline
Writing large arrays (buffers) to FLASH on dsPIC33 processors
2008/01/10 18:36:25
(permalink)
although there is a brief example of how to use the commands _erase_flash(), _write_flash16() and _write_flash24() that were added in C30 v3.01. This example shows how to write arrays that exceed the page boundary: // Flash_Write Test_011008.c // // A test for demonstrating how to write a large array to FLASH (Program Memory) // on the dsPIC33FJ256GP710 processor installed in the Explorer16 development // board. Objective: Define and write an array of 2048 16 bit words to FLASH. #include "libpic30.h" #include "p33Fxxxx.h" // _FLASH_PAGE is a static definition (512 for the dsPIC33). // _FLASH_ROW is a static definition (64 for the dsPIC33). // Define an array of 2048 words in program memory. int FLASH_data[_FLASH_PAGE*4] __attribute__((space(prog),aligned(_FLASH_PAGE*8))); int main() { int data_index; int page_index; int row_index; int Test_data[_FLASH_ROW]; unsigned long Flash_pointer; // initialize some data for this test for (data_index = 0; data_index < _FLASH_ROW; ) { Test_data[data_index] = data_index; data_index++; } // Get the address of the predefined variable(s)in program space. _init_prog_address(Flash_pointer, FLASH_data); // This outer loop is used to erase each page after the page boundary has been crossed. for (page_index = 0; page_index < 4; ) { _erase_flash(Flash_pointer); // erase a page. // The row level loop. 8 rows per page for the dsPIC33 for (row_index = 0; row_index < 8; ) { // Write each row here with 64 words of data. _write_flash16(Flash_pointer, Test_data); // increment the values for the test data before writing the next row. // NOTE: This is a post increment so it will increment once more // after the final row is written. for (data_index = 0; data_index < _FLASH_ROW; ) { Test_data[data_index] += 64; data_index++; } asm("nop"); // nops here for breakpoint placement. asm("nop"); asm("nop"); asm("nop"); // Increment the Flash_pointer by one row. Flash_pointer += (_FLASH_ROW * 2); // NOTE: No additional addressing action is required when // page boundaries are crossed. However, the page boundary // must be kept track of since the page erase function is // used prior to the writing of rows on a page. // Increment the row index. row_index++; } asm("nop"); // nops here for breakpoint placement. asm("nop"); asm("nop"); asm("nop"); // Increment the page index. page_index++; } asm("nop"); // Place Breakpoint here, then read the part to show data in FLASH. asm("nop"); asm("nop"); asm("nop"); }
post edited by ren - 2008/01/10 18:44:30
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
Using SHT11 on 16F628 in assembler
2008/01/21 16:40:06
(permalink)
; init code movlw 255 ; almeno 9 impulsi di clock con DATA=1 per reset SHT11... EXTENDED_CALL DoI2CMO movlw 255 EXTENDED_CALL DoI2CMO ; movlw 44 ; EXTENDED_CALL Delay_mS_free ; ritardo 11mS non necessario MY_PAGESEL main ; read movlw DELAY_I2C_SLOW movwf DelaySPIVal ; I2Cstart x SHT11... bsf PORTB,SPI_232_I ; imposto DATA=1 e CLK=0 EXTENDED_CALL setDataOutput ; OCCHIO a manipolare PORTB che e' I/O! (v. anche IRQ) EXTENDED_CALL Delay_SPI bsf PORTA,SPI_232_O ; CLK=1 EXTENDED_CALL Delay_SPI bcf PORTB,SPI_232_I ; DATA=0 ; data line goes low during high clock for start bit EXTENDED_CALL Delay_SPI bcf PORTA,SPI_232_O ; CLK=0 EXTENDED_CALL Delay_SPI bsf PORTA,SPI_232_O ; CLK=1 EXTENDED_CALL Delay_SPI bsf PORTB,SPI_232_I ; DATA=1 EXTENDED_CALL Delay_SPI bcf PORTA,SPI_232_O ; CLK=0 EXTENDED_CALL Delay_SPI movlw BuffI8Arg ; ...a partire da parm3... movwf FSR EXTENDED_CALL DoI2CMO_INDF ; mando INDF (address=cmd) ; return_code? in parm? MY_PAGESEL bytes51 decf BuffI6Arg,f ; se ce n'e' un altro... bz byte51_2 incf FSR,f EXTENDED_CALL DoI2CMO_INDF ; mando INDF MY_PAGESEL bytes51 byte51_2: ; questo VUOLE un ritardo tra WR e RD per la conversione (v. data sheet: 55-210mS) movfw BuffI8Arg xorlw 3 bz byte51_4_ xorlw 3 ^ 5 bnz byte51_4 ; MA SOLO in LETTURA TEMP/HUMID! (NO in impostazioni ecc.) ; oppure aspettare che SDI scenda... byte51_4_: movlw 5 movwf temp2 byte51_5: movlw 200 ; 50mS ca. EXTENDED_CALL Delay_mS_free MY_PAGESEL bytes51 decfsz temp2,f goto byte51_5 byte51_4: movlw 0xff movwf parm1 movwf parm2 movfw BuffI7Arg ; se devo ricevere... bz byte51_3 ; (se no, potrei anche dare ACK semplice... o return_code del WRITE) decf BuffI7Arg,w ; indico se ACK (Buff6=1 -> W=0) EXTENDED_CALL DoI2CMI MY_PAGESEL bytes51 movwf parm1 decf BuffI7Arg,f bz byte51_3 decf BuffI7Arg,w ; indico se ACK (Buff6=1 -> W=0) EXTENDED_CALL DoI2CMI MY_PAGESEL bytes51 movwf parm2 byte51_3: EXTENDED_CALL setDataOutput ; rimetto a posto (mancando I2Cstop qua...) bsf PORTB,SPI_232_I ; DATA=1 ; data goes high while clock high for stop bit EXTENDED_CALL Delay_SPI MY_PAGESEL bytes51 ; support routines DoI2CMO_INDF: movfw INDF DoI2CMO: ; Master, output (CLK negativo): entra in W il byte movwf temp movlw 8 movwf tempC call setDataOutput DoI2CMO_: ; clrwdt ; gia' in Delay_uS rlf temp,f ; MSB first btfss STATUS,C bcf PORTB,SPI_232_I ; DATA=0 btfsc STATUS,C bsf PORTB,SPI_232_I ; DATA=1 call Delay_1uS ; serve un minimo di ritardo tra il settaggio di DATA e la salita di CLK bsf PORTA,SPI_232_O call Delay_SPI bcf PORTA,SPI_232_O call Delay_SPI decfsz tempC,f goto DoI2CMO_ call setDataInput call Delay_SPI call setClockHigh ; aspetto ACK ; Per WAIT_STATE dello slave (CLK basso)... NON e' chiaro se PRIMA o DOPO ACK... (PicBell lo fa dopo!) ; questo lo controlla SEMPRE! call Delay_SPI ; dopo Delay, qua arrivo con W=0 e Z=1 btfsc PORTB,SPI_232_I addlw -1 ; Z=1 se ACK=OK (basso), altrimenti Z=0 e W!=0 bcf PORTA,SPI_232_O return DoI2CMI: ; Master, input (CLK negativo): esce in W il byte se C=0 o C=1=errore ; entra W=1 se bisogna dare ACK allo slave o 0 se no movwf temp2 movlw 8 movwf tempC call setDataInput DoI2CMI_: ; clrwdt ; gia' in Delay_uS call Delay_SPI ; call setClockHigh ; CLK=1 fare? boh? bsf PORTA,SPI_232_O call Delay_SPI ; btfss PORTB,SPI_232_I ; inutile... bcf STATUS,C btfsc PORTB,SPI_232_I bsf STATUS,C rlf temp,f ; MSB first bcf PORTA,SPI_232_O decfsz tempC,f goto DoI2CMI_ call setDataOutput movf temp2,f ; invio ACK come richiesto (Z=1 se stop cioe' ACK=1, Z=0 cioe' ACK=0) btfss STATUS,Z bcf PORTB,SPI_232_I ; DATA=0 btfsc STATUS,Z bsf PORTB,SPI_232_I ; DATA=1 bsf PORTA,SPI_232_O call Delay_SPI bcf PORTA,SPI_232_O call Delay_SPI movfw temp return setDataOutput: bsf STATUS,RP0 ; Bank 1 bcf TRISB,SPI_232_I ; DATA e' output bcf STATUS,RP0 ; Bank 0 return (to be edited for clarity...)
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
Basic code for a Stepper Motor on PIC18F2420
2008/02/05 14:00:40
(permalink)
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
Software PWM to dim Leds, in assembler for 16F628:
2008/04/07 12:08:01
(permalink)
Software PWM to dim Leds, in assembler for 16F628: ORG 0x004 ; interrupt vector location movwf w_temp ; save off current W register contents movfw STATUS ; move status register into W register movwf status_temp ; save off contents of STATUS register btfss INTCON,T0IF ; Timer 0 goto EndISR int_TMR0: clrf STATUS ; bank 0 bcf INTCON,T0IF ; clear bit IRQ movlw TMR0BASE movwf TMR0 ; re-inizializzo TMR0 movfw Timer64RGB ; gestisco i livelli PWM R-G-B subwf RVal,w btfss STATUS,C bsf myPortB,RPWMOBit movfw Timer64RGB subwf GVal,w btfss STATUS,C bsf myPortB,GPWMOBit movfw Timer64RGB subwf BVal,w btfss STATUS,C bsf myPortB,BPWMOBit movfw myPortB movwf PORTB incf Timer64RGB,f btfss Timer64RGB,6 ; se >= 64... goto end_TMR0 movfw myPortB andlw LedOVal | I2CClkVal | TX_RXVal ; movlw LedOVal | I2CClkVal | TX_RXVal ; andwf myPortB,f movwf myPortB movwf PORTB clrf Timer64RGB incf Timer1,f ; il timer a 200Hz end_TMR0: EndISR: movfw status_temp ; retrieve copy of STATUS register movwf STATUS ; restore pre-isr STATUS register contents swapf w_temp,f swapf w_temp,w ; restore pre-isr W register contents retfie ; return from interrupt The above handles 3 channels (RGB led) at PORTB: the desired values are placed in RVal, GVal, and BVal, 8bit variables. Timer0 must be enabled to generate IRQs @ around 64*desired PWM frequency, i.e. circa 6400 Hz is ok on average.
post edited by DarioG - 2010/12/27 03:05:53
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
Software PWM to dim Leds, in C for 18F:
2008/04/07 12:10:23
(permalink)
Same thing in C, with C18, on a PIC18F such as 4520, 4550, 252, etc: void high_isr(void) { static byte i,j; // static byte Timer64RGB; messo sopra x ACCESSBANK if(INTCONbits.TMR0IF) { // Timer 0 .. INTCONbits.TMR0IF=0; // clear bit IRQ // WriteTimer0(TMR0BASE); // reinizializzo TMR0 // in questo modo evito overhead nell'interrupt... causa chiamata di funzione! TMR0L=TMR0BASE; // TMR0H=0; Timer64RGB++; Timer64RGB &= 0x7f; if(Timer64RGB < RGBValue[0][0]) m_RPWMO1Bit = 1; else m_RPWMO1Bit = 0; // m_RPWMO1Bit = Timer64RGB < RGBValue[0][0] ? 1 : 0; e' + veloce come sopra... if(Timer64RGB < RGBValue[1][0]) m_RPWMO2Bit = 1; else m_RPWMO2Bit = 0; if(Timer64RGB < RGBValue[2][0]) m_RPWMO3Bit = 1; else m_RPWMO3Bit = 0; if(Timer64RGB < RGBValue[3][0]) m_RPWMO4Bit = 1; else m_RPWMO4Bit = 0; if(Timer64RGB < RGBValue[4][0]) m_RPWMO5Bit = 1; else m_RPWMO5Bit = 0; if(Timer64RGB < RGBValue[5][0]) m_RPWMO6Bit = 1; else m_RPWMO6Bit = 0; if(Timer64RGB < RGBValue[6][0]) m_RPWMO7Bit = 1; else m_RPWMO7Bit = 0; if(Timer64RGB < RGBValue[7][0]) m_RPWMO8Bit = 1; else m_RPWMO8Bit = 0; Counter++; // m_Led2Bit ^= 1; //check timer } //if timer... } 8 leds are handled in here. A similar setup is used to the previous snippet of code.
post edited by DarioG - 2010/12/27 03:06:32
|
Xianthax
Starting Member
- Total Posts : 48
- Reward points : 0
- Joined: 2007/01/10 15:58:25
- Location: 0
- Status: offline
RE: Basic code for a Stepper Motor on PIC18F2420
2008/04/07 13:01:28
(permalink)
Fast sqrt or inverse sqrt approximation: Method and Credit to: http://www.mceniry.net/papers/Fast%20Inverse%20Square%20Root.pdf Issue at hand is a fast way to do float sqrt(float) or invsqrt to a reasonable accuracy... code: float fastSqrt(float x) { union { float f; unsigned long ul;} y; y.f = x; y.ul = (0xbe6eb50cul - y.ul ) >> 1; y.f = 0.5f * y.f * (3.0f - x * y.f * y.f ); //y.f = 0.5f * y.f * (3.0f - x * y.f * y.f ); //repeat iterations to achieve lower error //y.f = 0.5f * y.f * (3.0f - x * y.f * y.f ); //y.f = 0.5f * y.f * (3.0f - x * y.f * y.f ); //y.f = 0.5f * y.f * (3.0f - x * y.f * y.f ); //y.f ~= 1.0f/sqrt(x) return y.f * x; // sqrt(x) = x / sqrt(x), return just y.f if you need invsqrt(x) } runs in about 123us on a pic18 @ 41.66666mhz vs clib sqrt(x) function at about 604us, (mplab sim, 1 newton step). error functions can be found in the pdf listed about and newton steps can be added or subtracted as needed for accuracy...1 step yields max relative error <= ~.00175 i ran through the math far enough to find that doing a new version for sqrt(x) would not be faster to run than calculating 1.0/sqrt(x) and multiplying by x to get sqrt(x) as the newton step would require divisions. -x
|
DarioG
Allmächtig.
- Total Posts : 54081
- Reward points : 0
- Joined: 2006/02/25 08:58:22
- Location: Oesterreich
- Status: offline
Software USART (only TX) for 16F PICs.
2008/05/21 10:52:14
(permalink)
Software USART (only TX) for 16F PICs. ; --------------------------------------------------------------------- PutByte232_0: ; manda uno 0 clrw ; prosegue... ; al fondo c'e' un MOVLW/MOVWF per rimettere PORTB a posto (poiche' e' I/O) PutByte232: ; manda un byte movwf Data_AREA CLRF COUNT232 ;RESET 8 BIT COUNT #ifdef TX_BUFFERED BCF PORTB,TXComBit ;LOW RD FOR START BIT #else BsF PORTB,TXComBit ;LOW RD FOR START BIT #endif CALL Delay_Bit SendByte1: RRF Data_AREA, F ;SHIFT Data TO CARRY BTFSc STATUS,C ;0 / 1 ? #ifdef TX_BUFFERED BSF PORTB,TXComBit ;SEND A 1 #else BcF PORTB,TXComBit ;SEND A 1 #endif BTFSs STATUS,C ;1 / 0 ? #ifdef TX_BUFFERED BCF PORTB,TXComBit ;SEND A 0 #else BsF PORTB,TXComBit ;SEND A 0 #endif CALL Delay_Bit INCF COUNT232,F BTFSS COUNT232,3 ;COUNT = 8 ? GOTO SendByte1 #ifdef TX_BUFFERED BSF PORTB,TXComBit ;SEND STOP BIT #else BcF PORTB,TXComBit ;SEND STOP BIT #endif CALL Delay_Bit #ifdef TX_BUFFERED BSF PORTB,TXComBit ;SEND STOP BIT (un altro...) movlw TXComVal movwf PORTB ; IMPORTANTE,xche' PORTB e'in/out (PS/2) #else BcF PORTB,TXComBit ;SEND STOP BIT (un altro...) movlw 0 ; IMPORTANTE,xche' PORTB e' in/out (PS/2) movwf PORTB #endif GOTO Delay_Bit Should be self-explaining; the Delay_Bit has to be computed for a bit-time delay, say 104uSec for 9600baud. The "TX_BUFFERED" is defined when a MAX232 is used, and undefined otherwise (your case).
post edited by DarioG - 2010/12/27 03:05:32
|