• AVR Freaks

Hot!Harmony 3 configurator, exception when generating code

Author
swf
New Member
  • Total Posts : 14
  • Reward points : 0
  • Joined: 2015/05/06 12:47:08
  • Location: 0
  • Status: offline
2021/03/08 10:10:53 (permalink)
0

Harmony 3 configurator, exception when generating code

When generating code from the Harmony 3 configurator I get the following error "An exception occured during file preprocessing."  The console shows the following error:
FTL stack trace ("~" means nesting-related):
- Failed at: ${.vars["${SYS_TIME_PLIB?lower_case}"... [in template "system_config.h.ftl" at line 4, column 54]
 
I did not have problems the last time I had the project open.  The code will compile from MPLAB.

Attached Image(s)

#1

2 Replies Related Threads

    optimus_jack
    Senior Member
    • Total Posts : 113
    • Reward points : 0
    • Joined: 2017/02/16 03:02:47
    • Location: 0
    • Status: offline
    Re: Harmony 3 configurator, exception when generating code 2021/03/08 22:06:02 (permalink)
    0
    Hi,
    I am able to generate code with core Timer and Time system service on PIC32MZ EF.
    Can you attach the project so that i can have a look and see what might be the problem.
     
    Quick hint would be to remove Time system service from project graph and add it back and then connect to Core Timer
     
    You can refer to https://github.com/Microchip-MPLAB-Harmony/core_apps_pic32mz_ef/tree/master/apps/system/time/sys_time_multiclient
    #2
    swf
    New Member
    • Total Posts : 14
    • Reward points : 0
    • Joined: 2015/05/06 12:47:08
    • Location: 0
    • Status: offline
    Re: Harmony 3 configurator, exception when generating code 2021/03/12 13:56:18 (permalink)
    0
    I tried your suggestion and it worked.
    Thank you!
    #3
    Jump to:
    © 2021 APG vNext Commercial Version 4.5