USB Interface to windows 10 serial software
Hi. I want to interface PIC18F4550/2550 based circuit with some windows 10 serial software like maybe, hyperterminal or realterm using it's USB connection. Any idea and links on how to begin with. I have to use XC8 compiler.
Second option is to use USB to serial converter again it should be compatible with windows 10, is there any easily available module for that? In this case I can use any PIC microcontroller to interface.
Third option is to use Arduino UNO. Can I directly connect it with windows 10 serial softwares ( I know that UNO can be programmed directly through USB cable and vice versa may also be true to use it's USB to communicate with windows serial software?).
Please reply for all three options.