• AVR Freaks

Hot!ICD3 and PIC32MZ processors

Author
clivel
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2011/12/06 13:51:09
  • Location: 0
  • Status: offline
2021/02/24 12:40:00 (permalink)
0

ICD3 and PIC32MZ processors

Not having done any embedded development for a few years now, I am looking at a project in which the PIC32MZ0512EFK064 seems the most likely candidate. For development, I am hoping to use my MPLAB ICD3 which has been lying in a drawer untouched for ages.
So, a simple question that I can't seem to find the answer to, Does the ICD 3 support the PIC32MZ processors, and in particular the PIC32MZ0512EFK064?
I have looked, but haven't been able to find a list of processors supported by the ICD 3.
Thanks,
Clive
#1

3 Replies Related Threads

    du00000001
    Just Some Member
    • Total Posts : 4145
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: offline
    Re: ICD3 and PIC32MZ processors 2021/02/25 07:31:59 (permalink)
    +2 (2)
    According to my MPLAB X installation, the PIC32MZ0512EFK064 is supported by ICD3, PICKit3 and newer devices.

    PEBKAC / EBKAC / POBCAK / PICNIC (eventually see en.wikipedia.org)
    #2
    Mysil
    Super Member
    • Total Posts : 4130
    • Reward points : 0
    • Joined: 2012/07/01 04:19:50
    • Location: Norway
    • Status: offline
    Re: ICD3 and PIC32MZ processors 2021/02/25 08:01:18 (permalink)
    +3 (3)
    Hi,
     
    With each MPLAB X installation, there is a big file with details about programming and debug support for  microcontroller devices. 
    Somewhere like:
    "C:\Program Files\Microchip\MPLABX\v5.45\docs\Device Support.htm"
    or
    "C:\Program Files (x86)\Microchip\MPLABX\v5.25\docs\Device Support.htm"
     
        Mysil
    #3
    clivel
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2011/12/06 13:51:09
    • Location: 0
    • Status: offline
    Re: ICD3 and PIC32MZ processors 2021/02/25 15:09:43 (permalink)
    0
    Thanks du00000001 and Mysil,
    That is very helpful :)
    Clive
     
    #4
    Jump to:
    © 2021 APG vNext Commercial Version 4.5