Anobium
Very willing to post .S source/or a project, but, really looking for experience on MidRange ASM to PIC-AS program porting. Evan
Hola Evan
All in this post comes from my own experience and a bit of help from member dan1138 in this forum.
Ranting is not in my plan. What is gone, is gone and, if I mention something that you already know, it could help somebody else reading this in the future. I hope.
Worked in Assembler for many years (starting with PIC16C57) and I am not C conversant. Currently using Win 10, MPLABX 5.45, Assembler pic-as 2.31, PICkit 4 and 18F family. Last projects, maybe four or five, with the 18F2321.
---------------------------------------------------------------------------------------------------------------------------------
a) XC8 does not come bundled with MPLABX. You download XC8 later. It includes pic-as 2.31 assembly.
To work in Assembly, when starting a new project you select explicitly pic-as 2.31. Spent one full day trying with XC8 until I realized so.
Check the attached picture somewhere below.
b) Until meeting pic-as 2.20, relocatable mode did not exist for me.
Now, relocatable is the de-facto mode. You use ORG when you need to establish an absolute location, quite infrequent in common applications. I've seen somebody asking this, but trying to force the whole in aboslute mode is pure nonsense. Kiss it good bye and forget.
c) Until starting with pic-as 2.20, I had no idea of what the
Psect directive was.
Program sections (psect for short) group data or code. After struggling with the concept and actual usage, I managed to compile this list of predefined ones, which seems to cover most of it:
/* Psects du jour as suggested by the Chef:
Data in RAMFull: psect..udata,global,class=RAM,SPACE_DATA,delta=1,noexec
Use: Psect udata
Full: psect udata_acs,global,class=COMRAM,SPACE_DATA,delta=1,noexec
Use: Psect udata_acs
Full: psect udata_bank0,global,class=BANK0,SPACE_DATA,delta=1,noexec
Use: Psect udata_bank0
Full: psect..udata_bank1,global,class=BANK1,SPACE_DATA,delta=1,noexec
Use: Psect udata_bank1
Data in EEPROMUse: Psect eedata,global,class=EEDATA,space=SPACE_EEPROM,delta=2,noexec
Data in program memoryUse: Psect data,global,class=CONST,space=SPACE_CODE,delta=1,noexec
Code - absoluteUse: Psect code,abs,global,class=CODE,space=SPACE_CODE,delta=1,reloc=2
Code - relocatableFull: Psect code,global,class=CODE,space=SPACE_CODE,delta=1,reloc=2
Use: Psect code
Flags in RAM (Access bank)
Use: Psect bitflags,bit,global,space=SPACE_DATA,class=COMRAM
Flags in RAM (BANKX)
Use: Psect bitflags,bit,global,space=SPACE_DATA,class=BANKX
*/
d) In the XC8 PIC Assembler User's Guide for Embedded Engineers (current version - verified five day ago - the paragraph
7.2 Defining And Using Bits, explains how to define a bit object inside a specific Psect, fitting the "bit" flag which means "this Psect holds bit objects". Those objects are just 1 bit wide.
The guide shows these two examples for defining flag needCopy
BANKSEL (needCopy/8)bsf BANKMASK(needCopy/8),needCopy&7or
#define NEEDCOPY BANKMASK(needCopy/8),needCopy%7Please note that
mod 7 IS WRONG. The right divisor for it is
8, thus the proper calculation must be:
BANKSEL (needCopy/8)bsf BANKMASK(needCopy/8),needCopy mod 8or
#define NEEDCOPY BANKMASK(needCopy/8),needCopy mod 8I opened a ticket on this subject and MCHP acknowledged the error.
e) Related to the above, unless I find a reason / need to go that way, I define flags as follows:
;FLAGS;All flags are defined in Access, here.global FLAGS_TB,FLAGS_KPFLAGS_TB: DS 1FLAGS_KP: DS 1#define TBASE_FAST_ELAP FLAGS_TB,0#define TBASE_SLOW_ELAP FLAGS_TB,1#define KP_NEEDS_1stREAD FLAGS_KP,4#define KP_ENABLED FLAGS_KP,3f) Debugging - There is a flaw in debugging mode: the name of variables defined in absolute RAM location is not visible.
In spite of variables being duly defined with
DABS and made public using the global directive twice, they appear properly listed in the respective .lst file, with label and address; their values are visible in the GPRs block in "hex" or "symbol" format, but their label is
not shown.
The rest of the RAM variables do exhibit their value and name (label).
Opened a ticket on this subject; MCHP acknowledged the flaw.
g) Assembly Header file (otherwise known as "PIC 18F2321.inc")
To get the specific .inc file for your particular micro, go to (
in my PC at least, this is the right path):
C: \
Program files \ Microchip \ xc8 \ v2.31 \ pic \ include \ proc \
pic18f2321.inc - make sure you do not enter Program files (x86).
I recall someone posting that the old .inc file (MPASM) could be used. With the current micro, found one (or two?) register names altered so you must use the file in the path above.
Amongst other things, the directive #include <xc.inc>, allows the assembler to recognize psect's / memory spaces' names defined in the .inc file.
h) I strongly suggest you peruse the .inc file above in full. Make sure you read it down to the very end so you will understand what I am explaining in point g.
i) Porting existing projects was simple for me. After completing my first project with pic-as, I rewrote my whole library, in less than three days IIRC. After that I reworked my basic "template".
Hope some of this is useful to you.
post edited by atferrari - 2021/02/18 09:12:34
Attached Image(s)