• AVR Freaks

Hot!Include directory recursive search

Author
neworld
Junior Member
  • Total Posts : 102
  • Reward points : 0
  • Joined: 2011/03/04 14:18:23
  • Location: Calgary, Alberta, Canada
  • Status: offline
2021/01/29 14:15:42 (permalink)
0

Include directory recursive search

Is there a gcc command that I could use in the project properties 'C include dirs' dialog that would recursively search a directory. As it stands, each code module needs the sub-directory specified.
 
Example:
C:\firmware\project\libs
    code_module1
    code_module2
    code_module3
 
In the 'C include dirs' dialog:
libs\code_module1
libs\code_module2
libs\code_module2
 
I read something about using libs/**, but that does not work.
 
Thnx.
 
#1

0 Replies Related Threads

    Jump to:
    © 2021 APG vNext Commercial Version 4.5