Re: test
2021/01/27 15:00:09
(permalink)
☄ Helpfulby moser 2021/01/28 04:07:44
If you want to do a real test, do it from a PC that is NOT signed in to the Microchip corporate network.
It has been well established that the firewall causing most of the problems on this board is bypassed if you ARE signed in to the company network.
To get a useful answer, always state which PIC you are using!