• AVR Freaks

EZBL OTA via ESP

Author
gopz
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2021/01/07 01:43:59
  • Location: 0
  • Status: offline
2021/01/21 11:24:24 (permalink)
0

EZBL OTA via ESP

Hello Gentlemen,
 
I'm using custom board with PIC24FJ128GA306 with ex_boot_uart  implemented. I successfully done ex_app_led_blink exercise over FTP server/UART with ESP8266, but today the process crashed during PHASE 3. Something I noted about is that the application doesn't freeze as previous times and the process crashes because of TIMEOUT 00 00 EC FF.
 
Does anyone have an idea what's going on ? 
 
Regards,
 
Georgi Gospodinov 
#1

0 Replies Related Threads

    Jump to:
    © 2021 APG vNext Commercial Version 4.5