MCP 23s17 testing set-up problem/question
Hello I am experimenting with the MCP 23S17 expander, and have fabricated a circuit with a PIC 16F1516 mounted on one bread board with the serial connection made by a 8-line CAT5 cable to the 23s17 mounted on a second breadboard with LED's connected to the PORTA and PORTB pins as outputs.(I have no resisters in line with the LEDs) The 8 line cable supplies the cs, sck, and dat pins as well as a common ground and 5.1v vdd. The circuit operates as expected for a short while then it seems to freeze. I am just sending a series of byte values to step through the LEDs. When the freeze occurs all I have to do to unfreeze it is touch the MCP23s17 with my finger or sometimes just passing my hand near it will do the trick. Is there some capacitance problem I am having with my circuit? Any suggestions would be appreciated. John C