Odd MPLAB X issues - is it only me?
I'd like to know if anyone else is having the same problems with MPLAB-X so I know if it is my system or not:
Issue #1: About 20% of the time when I try to clean and build, it fails because some of the files that MPLAB generates are "locked". I have to use a file unlocker tool to delete them before I can work any more. I can't seem to find any specific things that cause this. But it is very frustrating and time consuming!
Issue #2: If I make a minor code change and then try to use 'Debug Main Project', what I get is the previous version - my change is not compiled in. I have to hit 'Clean and Build' every time before I can debug again.
Issue #3: About once an hour or so, I will be editing a file and the MPLAB-X program just disappears. It doesn't close, it just goes away. The process is just gone! Files are not saved but neither are they corrupted. I can run it again and it wakes up just fine and works just fine. Sometimes it will work for a few hours before this happens again.
My system is VERY solid and doesn't exhibit any issues like these doing anything else, nor did it have any problems with MPLAB-8. I uninstalled 5.45 and then reinstalled the whole thing, but the issues remain.
If anyone else has seen these behaviors please let me know.
Topher