• AVR Freaks

Hot!MCC I2C Slave Code/Hardware Issue

Author
jptalledo
Starting Member
  • Total Posts : 67
  • Reward points : 0
  • Joined: 2006/09/07 13:17:33
  • Location: 0
  • Status: offline
2020/12/23 04:09:34 (permalink)
0

MCC I2C Slave Code/Hardware Issue

Hi 
 
I am using the Microchip Curiosity LPC with a PIC16F15345. I enabled I2C Slave interface but the SCL pin is low and not allowing I2C to work correctly.
 
Checking the Curiosity LPC, RB6 (SCL) does not have any external pull-down/up. I am wondering why it is low level.
 
Also, Is there any guide/example on how to use the new I2C API functions?
 
On my code (attached) I only call I2C1_Open() but wondering if there is a good example of how to use the new API.
 
Thanks
 
 
 
post edited by jptalledo - 2020/12/23 04:25:41
#1

0 Replies Related Threads

    Jump to:
    © 2021 APG vNext Commercial Version 4.5