• AVR Freaks

Hot!RN4871- CTS GPIO

Author
ASICAlex
Starting Member
  • Total Posts : 50
  • Reward points : 0
  • Joined: 2018/02/27 15:40:02
  • Location: 0
  • Status: offline
2020/12/03 22:02:35 (permalink)
4 (1)

RN4871- CTS GPIO

Is it possible to change the CTS pin to an output and write a value to it?  In the datasheet it says the P0_0 is a digital I/O which is configured as the UART_CTS by default, as well as having the pullup enabled by default.  I could not find a command to change this particular IO via a UART command.  The command "|0, <hex8>, <hex8> allows to change the output of P1_2 and P1_3, but I do not see a way to change any other "GPIO".  I would like to disable the pullup and drive that pin low if possible.  Is there anyway to do this?
 
#1

1 Reply Related Threads

    RISC
    Super Member
    • Total Posts : 5906
    • Reward points : 0
    • Status: offline
    Re: RN4871- CTS GPIO 2020/12/04 02:53:07 (permalink)
    0
    Hi,
    There are apparently changes to flow control in the latest firmware (v1.41). Have you checked release notes ?
    https://www.microchip.com/forums/m1159273.aspx
    Regards

    For support make sure to check first here : http://microchipdeveloper.com
    There are hundreds of PIC, AVR, SAM...which one do YOU use ?
    #2
    Jump to:
    © 2021 APG vNext Commercial Version 4.5