• AVR Freaks

Hot!Curiosity PIC32Mz v2... WARNING! (INFO)

Author
ElRola
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2020/03/05 15:08:45
  • Location: 0
  • Status: offline
2020/12/02 15:14:44 (permalink)
5 (1)

Curiosity PIC32Mz v2... WARNING! (INFO)

Hi all.
 
- DO NOT use the arduino shield connector... the J407 is inverted, the silkscreen is not correct, haven't checked the rest.
I do not have any shield but man........ i was just trying to use the pins...
 
more info:
- Use MplabX 5.3 -> newer versions do not let you use the board. I think someone have pointed that you have to tweak MPLABX to make it work but I haven't tried.
 
Between this, ICD4 version that needs manual patch to work, Harmony annoying gigantic repo... nevermind... have a nice day.
 
Edited: PIC32MZ Curiosity V2
post edited by ElRola - 2020/12/02 16:24:48
#1

2 Replies Related Threads

    Antipodean
    Super Member
    • Total Posts : 1984
    • Reward points : 0
    • Joined: 2008/12/09 10:19:08
    • Location: Didcot, United Kingdom
    • Status: offline
    Re: Curiosity v2... WARNING! (INFO) 2020/12/02 16:15:57 (permalink)
    2 (1)
    Which Curiosity Board??? There are a whole heap of them.
     
     

    Do not use my alias in your message body when replying, your message will disappear ...

    Alan
    #2
    ElRola
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2020/03/05 15:08:45
    • Location: 0
    • Status: offline
    Re: Curiosity v2... WARNING! (INFO) 2020/12/02 16:22:45 (permalink)
    0
    Ups!-.. sorry, Curiosity PIC32MZ EF 2.0 Development Board
    #3
    Jump to:
    © 2021 APG vNext Commercial Version 4.5