• AVR Freaks

Hot!KSZ8895 as unmanaged/managed switch is not working.

Author
m_snaeem@hotmail.com
Junior Member
  • Total Posts : 106
  • Reward points : 0
  • Joined: 2020/07/10 10:54:03
  • Location: 0
  • Status: offline
2020/11/13 04:05:11 (permalink)
0

KSZ8895 as unmanaged/managed switch is not working.

Hello,

Ihave tried to create an unmanaged switch using ksz8895 ethernet switch IC.
but i can get connected with internet using switch.
i have tried to use it is as unmanaged switch in default setting but no success.
Board is getting 122mA current which is constant.
i have attached the Circuit diagram. 
Can any body help me to find the error.
#1

0 Replies Related Threads

    Jump to:
    © 2021 APG vNext Commercial Version 4.5