• AVR Freaks

Hot![SOLVED] MPLAB X 5.45 links not working

Author
Howard Long
Super Member
  • Total Posts : 840
  • Reward points : 0
  • Joined: 2005/04/04 08:50:32
  • Status: offline
2020/10/25 02:37:26 (permalink)
5 (1)

[SOLVED] MPLAB X 5.45 links not working

The links on the product page https://www.microchip.com/mplab/mplab-x-ide don't seem to work.
 

https://www.microchip.com/mplabx-ide-windows-installer

returns:
 

{"StatusCode":500,"Message":"Internal Server Error while processing request..."}

 
 
 
This seems to work:
 

 
http://ww1.microchip.com/downloads/en/DeviceDoc/MPLABX-v5.45-windows-installer.exe

 
 
#1

1 Reply Related Threads

    ric
    Super Member
    • Total Posts : 28993
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: [SOLVED] MPLAB X 5.45 links not working 2020/10/25 02:59:07 (permalink)
    -1 (1)
    It's working now.
    That version has only just been released. It can take a day or so for the links to propgate to all their worldwide servers.
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5