• AVR Freaks

Hot!microchip IPE download for windows 10

Author
MPaulHolmes
Junior Member
  • Total Posts : 96
  • Reward points : 0
  • Joined: 2009/10/31 10:52:40
  • Location: 0
  • Status: offline
2020/10/16 11:01:52 (permalink)
0

microchip IPE download for windows 10

Where can I download just the IPE for windows 10?  Or do I have to get like 10 gig of other stuff just to have it?
#1

3 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 18965
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: microchip IPE download for windows 10 2020/10/16 11:41:10 (permalink)
    0
    You can check how many things you can exclude from the 10 gig download when you run the installation.
    You might be able to exclude mplabx and only include IPE
    #2
    tech24x7
    Junior Member
    • Total Posts : 104
    • Reward points : 0
    • Joined: 2013/10/14 21:38:52
    • Location: 0
    • Status: offline
    Re: microchip IPE download for windows 10 2020/10/17 22:59:03 (permalink)
    0
    https://www.microchip.com/mplab/mplab-x-ide installer here @ 1GB its a common installer for IDE/ IPE
    While installing you can uncheck IDE and other device architecture which you don't need.
     
    #3
    crosland
    Super Member
    • Total Posts : 2046
    • Reward points : 0
    • Joined: 2005/05/10 10:55:05
    • Location: Warks, UK
    • Status: offline
    Re: microchip IPE download for windows 10 2020/10/18 10:33:38 (permalink)
    0
    Be careful which devices you exclude. The IPE will fail as it expects certain devices to be present at start up.
     
    It will not allow you to re-run the installer and install what you need. You will need to uninstall and start again or install it in a non-default location and run from there.
     
    The installer was designed by idiots.
     
    Have fun using it. The UI was designed by more idiots.
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5