• AVR Freaks

Hot!Microchip MFi Library for iAP2

Author
Christian Hoelzel
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2020/09/30 02:38:49
  • Location: 0
  • Status: offline
2020/10/15 08:20:34 (permalink)
0

Microchip MFi Library for iAP2

Hi there,
does anyone know whether there is a version of the "Microchip MFi Library for iAP2" newer than 4.00 (26 Oct 2012) available? I need to use it, but it was built with XC32 v1.11, which makes the contained object files incompatible with XC32 v1.40 or later, leading to a linker error.
 
I'm using the following setup:
  • MPLAB X IDE v5.30
  • MPLAB XC32 v2.30
  • MLA v2012-07-18
  • Harmony v2.06
  • PIC32MX470F512L
Thanks in advance,
Christian
post edited by Christian Hoelzel - 2020/10/15 08:23:01
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5