• AVR Freaks

Hot!Custom Bootloader and Harmony

Author
photonthunder
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2020/10/06 12:09:09
  • Location: 0
  • Status: offline
2020/10/12 08:22:39 (permalink)
0

Custom Bootloader and Harmony

I have a custom bootloader for my SAMD51 design.  I use Harmony to setup the peripherals and I see that it does have some bootloader options (mostly related to freeRTOS which I don't use in my design).  Is there anyway that I can create a custom Harmony object that could represent my bootloader, thus doing the linker setup automatically for me?
#1
Jump to:
© 2020 APG vNext Commercial Version 4.5