• AVR Freaks

Hot!EZBL issue: undefined reference to `_EZBL_ModifyROM'

Author
thoraz
Junior Member
  • Total Posts : 117
  • Reward points : 0
  • Joined: 2013/06/01 18:37:43
  • Location: 0
  • Status: offline
2020/10/05 07:14:24 (permalink)
2 (1)

EZBL issue: undefined reference to `_EZBL_ModifyROM'

I'm working with the EZBL on PIC24FJ128GB406 and the bootloader works fine. Now I'd like to use the emulated data EEPROM in flash as shown in the EZBL Hands-on Bootloading Exercise, but when compiling I get the following error:
 
build/bootloader/production/commands.o(.text+0x122): In function `.LBE9':
: undefined reference to `_EZBL_ModifyROM'
make[2]: *** [dist/bootloader/production/gravity.X.production.hex] Error 255
make[1]: *** [.build-conf] Error 2
make: *** [.build-impl] Error 2

 
The EZBL_ModifyROM function is in the EZBL_WriteROMObj define and I get the error above only if I try to use it. I don't think that it's a "include .h" problem cause all the other functions in the ezbl.h file work fine. 
 
Any suggestions?
#1

1 Reply Related Threads

    thoraz
    Junior Member
    • Total Posts : 117
    • Reward points : 0
    • Joined: 2013/06/01 18:37:43
    • Location: 0
    • Status: offline
    Re: EZBL issue: undefined reference to `_EZBL_ModifyROM' 2020/10/09 02:03:35 (permalink)
    1 (1)
    No one? LoL: LoL
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5