• AVR Freaks

Hot!PIC32MM0256GPM064 Family datasheet ERROR

Author
jesselackey
New Member
  • Total Posts : 16
  • Reward points : 0
  • Joined: 2010/06/11 23:13:06
  • Location: 0
  • Status: offline
2020/09/24 18:30:24 (permalink)
4.5 (2)

PIC32MM0256GPM064 Family datasheet ERROR

The memory map for the 256K part is wrong.
I used the numbers as given an lost a good hour+ on WTF is wrong in that I couldn't place arrays where I wanted them in C code, the linker kept saying it was out of the kseg0 range.  Because the datasheet gives the range as 16K!
C'mon MICROCHIP!!!
J
 

Attached Image(s)

#1

2 Replies Related Threads

    Mysil
    Super Member
    • Total Posts : 3809
    • Reward points : 0
    • Joined: 2012/07/01 04:19:50
    • Location: Norway
    • Status: online
    Re: PIC32MM0256GPM064 Family datasheet ERROR 2020/09/24 23:43:53 (permalink)
    5 (1)
    Hi,
    The same mistake is still present in revsion D of the datasheet, document DS60001387D-page 43.
     
        Mysil
    #2
    NKurzman
    A Guy on the Net
    • Total Posts : 18976
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: PIC32MM0256GPM064 Family datasheet ERROR 2020/09/25 00:27:20 (permalink)
    1 (1)
    The documentation people don’t look at the forum for reported mistakes.
    You’re going to have to put a support ticket in if you want to get it corrected.
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5