• AVR Freaks

Hot!In free version, XCLM is extremely slow (takes 10 to 30 minutes to process xclm -status)

Author
edesarrieu
New Member
  • Total Posts : 11
  • Reward points : 0
  • Joined: 2018/09/26 02:50:37
  • Location: 0
  • Status: offline
2020/09/21 05:16:13 (permalink)
5 (1)

In free version, XCLM is extremely slow (takes 10 to 30 minutes to process xclm -status)

Hello,
 
Since several month, when I nee to compile, with XC8 or XC16, compilation hangs and takes from 10 to 60 minutes...
 
In MPLAB X, I have "License Check operation timed out. Please check internet connectivity'.
In command line, if I run /opt/microchip/xc16/v1.35/bin/xclm -status, it takes several minutes to answer:
Microchip XC License Manager Version: 2.22
License Path: /opt/microchip/xclm/license//
        Product: rlm_roam Type: Workstation Version: 1.0 Mode: ?

 
The problem is that I have no license, so I do not understand why it wants to contact a license server, and the compilation time is not acceptable.
 
Any help appreciated...
 
P.S. I run MPLAB X v5.30 + XC16 v1.35 + XC8 v2.00 on a Debian 9 (stretch)
post edited by edesarrieu - 2020/09/21 05:18:15
#1

3 Replies Related Threads

    edesarrieu
    New Member
    • Total Posts : 11
    • Reward points : 0
    • Joined: 2018/09/26 02:50:37
    • Location: 0
    • Status: offline
    Re: In free version, XCLM is extremely slow (takes 10 to 30 minutes to process xclm -statu 2020/09/21 08:10:27 (permalink)
    +1 (1)
    I installed MPLAB X 5.40, no changes.
    I installed XC16 1.60, no changes.
     
    I don't know what to do :-(
    #2
    JPortici
    Super Member
    • Total Posts : 1167
    • Reward points : 0
    • Joined: 2012/11/17 06:27:45
    • Location: Grappaland
    • Status: offline
    Re: In free version, XCLM is extremely slow (takes 10 to 30 minutes to process xclm -statu 2020/09/21 08:20:39 (permalink)
    -2 (2)
    you may want to check your firewall/proxy
    you may have blocked all connections in/out going from MPLABX
    #3
    edesarrieu
    New Member
    • Total Posts : 11
    • Reward points : 0
    • Joined: 2018/09/26 02:50:37
    • Location: 0
    • Status: offline
    Re: In free version, XCLM is extremely slow (takes 10 to 30 minutes to process xclm -statu 2020/09/24 06:35:23 (permalink)
    +1 (1)
    Thank you for your help. No firewall configured, my PC is available easily from network on any port.
    Another PC on same network and with same MPLAB X had no problem.
     
    Today I tried compilation and it worked. No explanation, this made me loose much time, and it is still not terminated maybe.
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5