• AVR Freaks

SAM L11 and CEC1702 comparison

Author
PublicEnemy
New Member
  • Total Posts : 3
  • Reward points : 0
  • Status: offline
2020/09/19 07:24:58 (permalink)
0

SAM L11 and CEC1702 comparison

Hi there, I'm ineterested to a secure microcontroller and I'd like to buy an evaluation board to start tinkering with it, but the thing is that I'm not very shure which one to choose. I'm wondering, beyound the lack of an embedded flash on the CEC1702, which features are present in the SAM L11 and which one in the CEC1702. Is there a table to perform a side by side comparison? I know that the "Kastelo" projetc (a Monero hardware wallet) uses the CEC1702 and I'm wondering why they didn't choose the SAM L11: is there a use case where one is more suited than the other?

Thanks to anyone willingful to shed some light!
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5