• AVR Freaks

Hot!What happened? - Updates Required - These plugin(s) have installed a dependency update:

Author
RDS Cliff
Junior Member
  • Total Posts : 67
  • Reward points : 0
  • Joined: 2016/09/23 11:50:05
  • Location: 0
  • Status: offline
2020/09/10 21:33:09 (permalink)
5 (1)

What happened? - Updates Required - These plugin(s) have installed a dependency update:

I opened up MPLAB X IDE this morning and was greeted with a dialog box with the following:
 
These plugin(s) have installed a dependency update:
MPLAB Code Configurator
The following plugin(s) have critical updates for compatibility. These plugins must either be updated or disabled:
MPLAB Code Configurator
 
I've been running the same versions of MPLAB X (v5.35) and MCC (v3.95.0) for months now and suddenly there is a compatibility problem?  I don't update all the time to avoid problems like this.  Now compatibility problems occur spontaneously????  I'm supposed to release code in two weeks.  Everything seems stable and I shouldn't need MCC but if I do, I'll have to risk my company's future by installing new versions of tools to make changes???????
#1

8 Replies Related Threads

    davea
    Super Member
    • Total Posts : 375
    • Reward points : 0
    • Joined: 2016/01/28 13:12:13
    • Location: Tampa Bay FL USA
    • Status: offline
    Re: What happened? - Updates Required - These plugin(s) have installed a dependency updat 2020/09/10 22:52:27 (permalink)
    0
    did the same thing with MPLAB X (v5.30) 
    updated MCC to (v4.0.1 with a core of v4.75)
    latest core is v5.0.1
    first try failed to open
    second time it opened
    did not save it when closed....
    must backup first
    but you would think they would not force it on you unless it worked ????
    #2
    JPortici
    Super Member
    • Total Posts : 1168
    • Reward points : 0
    • Joined: 2012/11/17 06:27:45
    • Location: Grappaland
    • Status: offline
    Re: What happened? - Updates Required - These plugin(s) have installed a dependency updat 2020/09/11 02:38:15 (permalink)
    5 (1)
    The real problem is that something happened automatically without me consenting.
    That's no no.
     
    this update also broke compatibility with harmony and wouldn't let me run MPLABX until i updated both, even if i wasn't using those.
     
    Lost about an hour at work.
     
    Also, remember a couple of months ago when some screwup on microchip servers prevented everybody from being able to work for several hours?
    #3
    du00000001
    Just Some Member
    • Total Posts : 3973
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: offline
    Re: What happened? - Updates Required - These plugin(s) have installed a dependency updat 2020/09/11 02:38:37 (permalink)
    0
    Might be the "critical compatibility issues" result from some fancy Win10 update.
    Win10 is currently infamous for their updates - poor quality and cutting threads. A simple update of the java engine might result in issues with MCC.

    PEBKAC / EBKAC / POBCAK / PICNIC (eventually see en.wikipedia.org)
    #4
    jtzeng
    Super Member
    • Total Posts : 505
    • Reward points : 0
    • Joined: 2003/11/07 12:42:20
    • Status: offline
    Re: What happened? - Updates Required - These plugin(s) have installed a dependency updat 2020/09/11 07:41:41 (permalink)
    0
    I went through the same issue.
    Had to back the CORE down to 4.85 as 5.0.1 dropped 16Bit bootloader support.
    Also have found that a lot of CORE updates are breaking ADC(PIC24) and UART(PIC24) with either big changes or flat out errors in the code generated.
    Just because the code compiles does not mean the generated code works.
     

    John Zigrang
    JTZ Engineering, Inc.
    #5
    RDS Cliff
    Junior Member
    • Total Posts : 67
    • Reward points : 0
    • Joined: 2016/09/23 11:50:05
    • Location: 0
    • Status: offline
    Re: What happened? - Updates Required - These plugin(s) have installed a dependency updat 2020/09/15 19:15:52 (permalink)
    0
    So no explanation from Microchip?  I guess I'll have to call them.  Stuck on a last minute bug right now.  Why does it always happen this way?
    #6
    RDS Cliff
    Junior Member
    • Total Posts : 67
    • Reward points : 0
    • Joined: 2016/09/23 11:50:05
    • Location: 0
    • Status: offline
    Re: What happened? - Updates Required - These plugin(s) have installed a dependency updat 2020/10/15 22:39:32 (permalink)
    0
    I have an open case with Microchip support for this bug.  It's been 5 weeks now.  Just got a message today saying they are still looking at it.
    I'm in the middle of code freeze for a medical device and I need to save the tools that I built the code with. Doesn't make sense to archive tools that don't even work.
    #7
    katela
    Super Member
    • Total Posts : 1876
    • Reward points : 0
    • Joined: 2013/06/11 05:25:18
    • Location: South Africa
    • Status: offline
    Re: What happened? - Updates Required - These plugin(s) have installed a dependency updat 2020/10/16 06:45:07 (permalink)
    0
    You can still load an earlier core v.4.x.x that's compatible with old libraries.

    Free online Microcontroller Tutorials and Projects for Hobbyists and students. From beginners to advanced. Website: www.studentcompanion.co.za
    YouTube Tutorials: https://www.youtube.com/StudentCompanionSA
    #8
    jtzeng
    Super Member
    • Total Posts : 505
    • Reward points : 0
    • Joined: 2003/11/07 12:42:20
    • Status: offline
    Re: What happened? - Updates Required - These plugin(s) have installed a dependency updat 2020/10/16 06:48:33 (permalink)
    0
    Have you taken this to your local FAE??  I find that after I open a case that I need help with they can help set a priority on it.
    Also I have found that the Pack Update have help, but for me the auto install is not working.
    I have to open the Pack window and install then one at a time. This solved my last auto update that caused a programming issue with the PICKIT4 on only 1 part number that I was using.
     
    It is hard to think that an auto update that has caused your problem did not install every thing you need, but it is happening.
    Good luck
     

    John Zigrang
    JTZ Engineering, Inc.
    #9
    Jump to:
    © 2020 APG vNext Commercial Version 4.5