• AVR Freaks

Hot!Is there anything related to RTOS in the microchip blockset?

Author
Poley
Starting Member
  • Total Posts : 54
  • Reward points : 0
  • Joined: 2020/06/16 08:39:05
  • Location: 0
  • Status: offline
2020/08/14 02:08:15 (permalink)
2 (1)

Is there anything related to RTOS in the microchip blockset?

I am looking to set up my model at different rates/priorities so I am assuming that I need to use RTOS to do this. 

Do the microchip blocks support this?
 
Thanks!
#1

1 Reply Related Threads

    Lubin
    Moderator
    • Total Posts : 447
    • Reward points : 5
    • Joined: 2007/03/31 07:38:15
    • Location: Bayonne, France
    • Status: offline
    Re: Is there anything related to RTOS in the microchip blockset? 2020/09/10 00:09:03 (permalink)
    0
    Hi Poley, 
     
    Yes, the microchip blocks implement multirate model either using single or multi-tasking. By default, the implementation is multi-tasking which implement the monotonic rate scheduler. No need for an RTOS.
     
    You might find furhter input on the forum (here for example https://www.microchip.com/forums/FindPost/1120678) and from Simulink help.
     
    Lubin
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5