• AVR Freaks

Hot!Cheap Target Board for PICKIT 3 not working.

Author
SeanD
Super Member
  • Total Posts : 479
  • Reward points : 0
  • Joined: 2009/10/23 07:48:32
  • Location: Dark Rural Northumberland
  • Status: offline
2020/08/14 00:26:39 (permalink)
0

Cheap Target Board for PICKIT 3 not working.

It has been some time since I posted. I have been using a Matrix Multimedia programmer which works well but only on Windows. I am now working mainly on OSX and remembered I had an old PICkit 3, but no suitable target board. The PICkit 3 seems to be still working.
 
I am using MPLAB IDE/IPE V5.4 and IPE recognises the PICkit3:
 
Connecting to MPLAB PICkit 3...

Currently loaded firmware on PICkit 3
Firmware Suite Version.....01.56.07
Firmware type..............Midrange
Target device was not found (could not detect target voltage VDD). You must connect to a target device to use PICkit 3.
 
The target board is a cheap one off Ebay: https://www.ebay.co.uk/it...d=p2060353.m2749.l2648
with minimal documentation.
 
I have tried a variety of PICs including a 40 pin 16F877 which I hoped would be foolproof, as the chip can't be placed incorrectly, but no PIC variety seems to work. 
 
I attach a photo. The immediate error seems to be: No target VDD but the board has no power supply?
 
Any ideas?
 

Attached Image(s)

#1

6 Replies Related Threads

    ric
    Super Member
    • Total Posts : 28378
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: Cheap Target Board for PICKIT 3 not working. 2020/08/14 01:06:57 (permalink)
    +2 (2)
    SeanD
    ...
    The immediate error seems to be: No target VDD but the board has no power supply?



    The default in IPE is for the programmer NOT to supply power.
    You have to enable "Advanced" mode, and go to the "Power" page to enable power to the target.

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    SeanD
    Super Member
    • Total Posts : 479
    • Reward points : 0
    • Joined: 2009/10/23 07:48:32
    • Location: Dark Rural Northumberland
    • Status: offline
    Re: Cheap Target Board for PICKIT 3 not working. 2020/08/14 01:21:28 (permalink)
    0
    Thanks, Will try. Sadly today the IPE keeps crashing before it is even loaded. The IDE seems to be working fine so a bit strange.
    #3
    SeanD
    Super Member
    • Total Posts : 479
    • Reward points : 0
    • Joined: 2009/10/23 07:48:32
    • Location: Dark Rural Northumberland
    • Status: offline
    Re: Cheap Target Board for PICKIT 3 not working. 2020/08/18 06:35:03 (permalink)
    0
    I thought a quick update might be useful. I have been totally unsuccessful at getting IPE V 5.4 to work again on OSX High Sierra. Even though it worked initially for a few hours it crashes predictably and repeatably about 2/3 way through loading. Even totally uninstalling and reinstalling V5.4 did not work.
     
    However, V 4.2 does work
     
    I have had success for 8 pin, 18 pin 28 pin and 40 pin chips.
    #4
    du00000001
    Just Some Member
    • Total Posts : 3946
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: offline
    Re: Cheap Target Board for PICKIT 3 not working. 2020/08/18 07:12:40 (permalink)
    +1 (1)
    I have a similar device. The issue yours may have as well: NO capacitor on the board.
    Adding a cap between VDD and GND really improved the performance.

    PEBKAC / EBKAC / POBCAK / PICNIC (eventually see en.wikipedia.org)
    #5
    DevMod1
    Administrator
    • Total Posts : 532
    • Reward points : 0
    • Joined: 2009/02/10 09:34:30
    • Location: 0
    • Status: offline
    Re: Cheap Target Board for PICKIT 3 not working. 2020/08/18 09:30:15 (permalink)
    0
    Please make sure when using MPLAB X v5.40 that you update the Tool Packs as they have firmware bug fixes.  Goto Tools->Packs then select the Tool Pack tab and update the pack for the tool you are using.
     

    _____________________________

    Please read the forum posting guidelines. Do not double post, please help keep these forums professional and comments respectful.
    Please notify the moderators of problems/spam/trolls.
    #6
    SeanD
    Super Member
    • Total Posts : 479
    • Reward points : 0
    • Joined: 2009/10/23 07:48:32
    • Location: Dark Rural Northumberland
    • Status: offline
    Re: Cheap Target Board for PICKIT 3 not working. 2020/08/19 00:35:02 (permalink)
    +1 (1)
    DevMod1
    thanks, I have updated all the tool packs but it has not resolved the issue. I have sent an automatically generated crash report to Apple a few times.
    #7
    Jump to:
    © 2020 APG vNext Commercial Version 4.5