• AVR Freaks

AnsweredHot!Clean project (without rebuilding)?

Author
rdpoor
Junior Member
  • Total Posts : 25
  • Reward points : 0
  • Joined: 2019/06/08 02:17:19
  • Location: 0
  • Status: offline
2020/08/09 07:35:55 (permalink)
0

Clean project (without rebuilding)?

I'm running MPLAB X v5.35.
 
How do you ask MPLAB to clean a project without rebuilding it?  (For example, when you're about to zip a project directory to send to somebody else...)
 
#1
andersm
Super Member
  • Total Posts : 2840
  • Reward points : 0
  • Joined: 2012/10/07 14:57:44
  • Location: 0
  • Status: offline
Re: Clean project (without rebuilding)? 2020/08/09 07:40:47 (permalink) ☼ Best Answerby rdpoor 2020/08/09 08:08:37
+2 (2)
Right-click on the project in the Projects tab, Clean. Right-click, Package will create a zip of the project for you.
#2
Jim Nickerson
User 452
  • Total Posts : 6736
  • Reward points : 0
  • Joined: 2003/11/07 12:35:10
  • Location: San Diego, CA
  • Status: online
Re: Clean project (without rebuilding)? 2020/08/09 07:44:55 (permalink)
+2 (2)
I use Production, Batch Build, select the project and click the Clean button.
#3
moser
Super Member
  • Total Posts : 587
  • Reward points : 0
  • Joined: 2015/06/16 02:53:47
  • Location: Germany
  • Status: offline
Re: Clean project (without rebuilding)? 2020/08/11 08:55:31 (permalink)
+1 (1)
I just press the broom symbol in the tool bar, which says: "Clean Project (PROJECTNAME)".
 
Note: I can do this because I customized my toolbar. You can do this by doing right-click at the toolbar and selecting "Customize". 
#4
Jump to:
© 2020 APG vNext Commercial Version 4.5