• AVR Freaks

Hot!Downloading firmware using PSCP protocol. Has anyone done this on PIC32?

Author
CRuff
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2008/10/27 14:48:14
  • Location: 0
  • Status: offline
2020/08/06 09:59:58 (permalink)
4 (1)

Downloading firmware using PSCP protocol. Has anyone done this on PIC32?

I have a requirement that my PIC32MZ bootloader accept firmware in PSCP format. I believe this is a secure method of downloading firmware using Putty.  Does anyone have knowledge of this protocol? I am not using operating systems in my PIC32MX or PIC32MZ designs. Thanks, Chris
#1

4 Replies Related Threads

    friesen
    Super Member
    • Total Posts : 2150
    • Reward points : 0
    • Joined: 2008/05/08 05:23:35
    • Location: Indiana, USA
    • Status: offline
    Re: Downloading firmware using PSCP protocol. Has anyone done this on PIC32? 2020/08/07 12:38:21 (permalink)
    5 (1)
    You'll have to buy wolfSSH, or build and MIT open source us something SSH.
     
    Who created the requirement?  There are other methods that will be simpler and cheaper, and probably just as secure.

    Erik Friesen
    #2
    NKurzman
    A Guy on the Net
    • Total Posts : 18908
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: Downloading firmware using PSCP protocol. Has anyone done this on PIC32? 2020/08/08 13:52:49 (permalink)
    4 (1)
    Harmony now includes wolfSSL
    #3
    CRuff
    New Member
    • Total Posts : 6
    • Reward points : 0
    • Joined: 2008/10/27 14:48:14
    • Location: 0
    • Status: offline
    Re: Downloading firmware using PSCP protocol. Has anyone done this on PIC32? 2020/08/12 09:26:03 (permalink)
    0
    this is RFQs from a military subcontractor. I am assuming that Harmony 3.x is the version that incorporates Wolf. So far I have used 2.06 successfully. Will check out the specs on the newer Harmony that supports Wolf.
     
    Thanks for your responses. Very helpful
     
    Chris
     
    #4
    NKurzman
    A Guy on the Net
    • Total Posts : 18908
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: Downloading firmware using PSCP protocol. Has anyone done this on PIC32? 2020/08/12 11:59:12 (permalink)
    0
    Harmony 2.06 also has WolfSSL.  Depending how V3.XX goes for you new project.
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5