• AVR Freaks

Hot!Redefining SPI pins on a PIC32MM0064GPL020

Author
Bad Steve
Starting Member
  • Total Posts : 37
  • Reward points : 0
  • Joined: 2006/07/28 08:35:59
  • Location: 0
  • Status: offline
2020/08/04 13:40:34 (permalink)
0

Redefining SPI pins on a PIC32MM0064GPL020

Good Afternoon,
 
I have never run into this situation before and I am just looking for some clarification. I want to use the SPI2 function in the PIC32MM0064GPL020 and connect it to AD7398 D/A. The AD7398 does not have a SDO pin, so I cannot read anything out. Using MCC of MPLAB X, I want to redefine the SPI2 ports which I have. Do I have to define a SDI pin on the processor to a pin not in use? Will the processor be ok without anything defined as SDI? Thanks for your help.

Thanks in advance
Steve
#1

2 Replies Related Threads

    Bad Steve
    Starting Member
    • Total Posts : 37
    • Reward points : 0
    • Joined: 2006/07/28 08:35:59
    • Location: 0
    • Status: offline
    Re: Redefining SPI pins on a PIC32MM0064GPL020 2020/08/04 13:42:17 (permalink)
    0
    Sorry I think I posted this in the wrong forum

    Thanks in advance
    Steve
    #2
    ric
    Super Member
    • Total Posts : 28378
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: offline
    Re: Redefining SPI pins on a PIC32MM0064GPL020 2020/08/04 13:45:23 (permalink)
    0
    Question has been reposted to https://www.microchip.com/forums/m1149590.aspx
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5