• AVR Freaks

Hot!Licence Check operation timed out

Author
marelcom
Starting Member
  • Total Posts : 40
  • Reward points : 0
  • Joined: 2018/01/17 03:18:47
  • Location: 0
  • Status: offline
2020/08/03 07:00:54 (permalink)
5 (1)

Licence Check operation timed out

Hi
 
since a few weeks thers shows up this popup message:
 Attachments are not available: Download requirements not met
 
 
- MPLABX: v5.40
- XC32: v2.20 (free) / v2.40 (free)
- XC8: v2.05 (pro)
 
For XC8 i have a pro licences. But XC32 I use only as free version.
Does anybody know why this pop up is showing up for XC32?

thanks and best regards
Markus
 

Attachment(s)

Attachments are not available: Download requirements not met
#1

4 Replies Related Threads

    marelcom
    Starting Member
    • Total Posts : 40
    • Reward points : 0
    • Joined: 2018/01/17 03:18:47
    • Location: 0
    • Status: offline
    Re: Licence Check operation timed out 2020/08/05 05:59:53 (permalink)
    +1 (1)
    PS: Clean and Built time with XC32 v2.2 is around 30 seconds
    Clean and Built time with XC32 v2.41 is around 10 minutes
    Compared by building the same project.
     
    Is there a dependency between the Licence timed out Error Message and this very slow built time?
    #2
    RISC
    Super Member
    • Total Posts : 5776
    • Reward points : 0
    • Status: offline
    Re: Licence Check operation timed out 2020/08/05 07:44:06 (permalink)
    +1 (3)
    Hi,
    You should post a ticket to Microchip online support to get some help on this
    Regards

    For support make sure to check first here : http://microchipdeveloper.com
    There are hundreds of PIC, AVR, SAM...which one do YOU use ?
    #3
    Swaroop Bekal
    Senior Member
    • Total Posts : 158
    • Reward points : 0
    • Joined: 2007/07/26 22:53:07
    • Location: Microchip Technology
    • Status: offline
    Re: Licence Check operation timed out 2020/08/07 07:36:36 (permalink)
    +1 (3)
    Can you unplug the network cable and switch-off WiFi and check if you see the same issue ?
    #4
    marelcom
    Starting Member
    • Total Posts : 40
    • Reward points : 0
    • Joined: 2018/01/17 03:18:47
    • Location: 0
    • Status: offline
    Re: Licence Check operation timed out 2020/08/12 07:54:19 (permalink)
    +1 (1)
    Thanks for your replay.

    No it does not help. Without a network connection, the timeout popup do still pop up for XC8, XC16 and XC32
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5