• AVR Freaks

MCP9600 - temperature reading

Author
tozito
New Member
  • Total Posts : 8
  • Reward points : 0
  • Joined: 2011/06/27 02:16:10
  • Location: 0
  • Status: offline
2020/07/24 05:20:56 (permalink)
0

MCP9600 - temperature reading

hi!
I've got a simple application with this MCP9600, I can read/write registers, but do not clearly understand how to read the temperature of the thermocouple.
I've attached a type K thermocouple, and configure it on register. Also did several reading tests with different config; but what's the temperature of the thermocouple I shouldread? do I only need to read the Hot junction temp (TH)?
or do I also need to read Delta + Cold temp and do some math?
Also what can we do with the raw ADC value? how to convert to temp?
Thanks to all.
#1

1 Reply Related Threads

    Jim Nickerson
    User 452
    • Total Posts : 6722
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: online
    Re: MCP9600 - temperature reading 2020/07/24 06:51:28 (permalink)
    0
    I found the data sheet provides a lot of information about interacting with this chip.
    I have been experimenting with the ESP32 and found this software provides an example of getting the temperature https://github.com/sparkfun/SparkFun_MCP9600_Arduino_Library/blob/master/src/SparkFun_MCP9600.cpp
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5