• AVR Freaks

[Libero SOC v12.4] Igloo2 creative board programmer not found error

Author
umeshD
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2020/07/15 00:03:23
  • Location: 0
  • Status: offline
2020/07/22 08:54:27 (permalink)
0

[Libero SOC v12.4] Igloo2 creative board programmer not found error

I am using Igloo2 creative development board
 (board link:https://www.microsemi.com/existing-parts/parts/143948)
 
I am trying to program the fpga with a new logic developed using Libero SOC v12.4, bitstream
is getting successfully generated but when I try to program the device the following error is shown
in log (Error: No programmers found. Please check the programmer connection to the computer
and ensure the drivers are properly installed.)
 
In Device Manager window (OS windows10) shows 4 devices under USB FP5 Serial Converter A,B,C,and D
but showing with following error (Windows cannot load the device driver for this hardware. The driver may be corrupted or missing. (Code 39))
 
Can anyone suggest the solution?
Thanks 
 
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5