• AVR Freaks

MPLAB 8.92 device selection

Author
Colormaker
Junior Member
  • Total Posts : 94
  • Reward points : 0
  • Joined: 2006/07/14 06:41:35
  • Location: 0
  • Status: offline
2020/07/15 13:55:11 (permalink)
0

MPLAB 8.92 device selection

I am setting up to use pic18lf2331 device on mplab 8.92 with icd3 deivce is on its own power. the device selection does not have the LF version can I use the pic18f2331 ? I will power the device at 3.3 volts.
#1

2 Replies Related Threads

    ric
    Super Member
    • Total Posts : 27954
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: offline
    Re: MPLAB 8.92 device selection 2020/07/15 15:14:55 (permalink)
    4 (2)
    Yes, just set it to the non-LF version. The programming protocol is the same.
    The LF chip is happy to run at 5V too.
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    Colormaker
    Junior Member
    • Total Posts : 94
    • Reward points : 0
    • Joined: 2006/07/14 06:41:35
    • Location: 0
    • Status: offline
    Re: MPLAB 8.92 device selection 2020/07/15 15:17:38 (permalink)
    0
    Thank you
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5