• AVR Freaks

Hot!Is there support for the dsPIC33FJ on the MCC yet?

Author
LJM
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2010/09/27 12:11:05
  • Location: 0
  • Status: offline
2020/07/15 03:39:33 (permalink)
0

Is there support for the dsPIC33FJ on the MCC yet?

I'm using a DSPIC33FJ128GP708A in  a project & would like to use the MCC.
 
Is there a device for it?
#1

2 Replies Related Threads

    du00000001
    Just Some Member
    • Total Posts : 3942
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: offline
    Re: Is there support for the dsPIC33FJ on the MCC yet? 2020/07/31 12:48:23 (permalink)
    5 (1)
    If you cannot find the DSPIC33FJ128GP708A in the device list, there is "no device for it".
     
    Too-old devices are not supported and will not be supported in the future. (Just to preempt you asking.)

    PEBKAC / EBKAC / POBCAK / PICNIC (eventually see en.wikipedia.org)
    #2
    RISC
    Super Member
    • Total Posts : 5776
    • Reward points : 0
    • Status: offline
    Re: Is there support for the dsPIC33FJ on the MCC yet? 2020/08/05 07:37:35 (permalink)
    0
    Hi,
    If you want to use MCC you could use a newer device which has the same features + some more advanced / new ones mostly compatible with DSPIC33FJ128GP708A : dsPIC33CK256MP508
    It dissipates less ( @ same speed) and has a lower cost too
    Regards

    For support make sure to check first here : http://microchipdeveloper.com
    There are hundreds of PIC, AVR, SAM...which one do YOU use ?
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5