• AVR Freaks

Hot!PPS for PIC18F46Q10

Author
PaulF
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2020/07/10 03:46:24
  • Location: 0
  • Status: offline
2020/07/11 01:38:01 (permalink)
0

PPS for PIC18F46Q10

Hi there. This query is concerned with Peripheral Pin Select for a PIC18F46Q10. Is it possible to redirect any LATxy output to any other LATxy output using PPS? For example, can I redirect LATA4 to LATB7? The data sheet has a RxyPPS code of 0x00 for LATxy but hasn't clear instructions about how to proceed. That might be because it is not possible! Thanks.
#1

2 Replies Related Threads

    Jerry Messina
    Super Member
    • Total Posts : 540
    • Reward points : 0
    • Joined: 2003/11/07 12:35:12
    • Status: offline
    Re: PPS for PIC18F46Q10 2020/07/13 11:54:02 (permalink)
    +2 (2)
    PaulF
    Is it possible to redirect any LATxy output to any other LATxy output using PPS? For example, can I redirect LATA4 to LATB7? The data sheet has a RxyPPS code of 0x00 for LATxy but hasn't clear instructions about how to proceed.

    Not possible.
     
    The RxyPPS = 0x00 is used to (re)assign the pin to the PORT instead of a peripheral.
    #2
    mpgmike
    Super Member
    • Total Posts : 450
    • Reward points : 0
    • Joined: 2014/01/23 17:27:06
    • Location: NJ
    • Status: offline
    Re: PPS for PIC18F46Q10 2020/07/15 16:59:22 (permalink)
    +1 (1)
    Chances are you could use CLC to duplicate or redirect outputs.

    I don't need the world to know my name, but I want to live a life so all my great-grandchildren proudly remember me.
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5