• AVR Freaks

Hot!Is the PIC32MZ DSP Library still under development?

Author
adown
New Users
  • Total Posts : 60
  • Reward points : 0
  • Joined: 2017/10/19 16:09:17
  • Location: Calgary
  • Status: offline
2020/07/08 15:41:29 (permalink)
5 (1)

Is the PIC32MZ DSP Library still under development?

Good morning, a question for anyone with visibility into Microchip:
Is the PIC32MZ DSP library currently being expanded?  Compared to the CMSIS libraries for ARM its very limited.  For example the only LMS adaptive filter implementation in the PIC32 library is 16-bit Q15 input, which CMSIS offers LMS implementations in 16-bit, and 32-bit (both float and Q31!).
 
-A
#1

1 Reply Related Threads

    JasonK
    Moderator
    • Total Posts : 3411
    • Reward points : 0
    • Joined: 2003/11/14 09:49:40
    • Location: Microchip Technology in Arizona, USA
    • Status: offline
    Re: Is the PIC32MZ DSP Library still under development? 2020/07/21 16:27:15 (permalink)
    0
    The DSP library packaged with the compiler isn’t being further developed, but there is a DSP library that is part of Harmony that provides additional functionality.

    Jason Kajita
     Follow me on Twitter
    http://support.microchip.com for urgent questions
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5