• AVR Freaks

Hot!How do I tell make not to make the hex file in the "Extra Loadables"

Author
jstout
New Member
  • Total Posts : 5
  • Reward points : 0
  • Joined: 2019/08/14 06:56:38
  • Location: 0
  • Status: offline
2020/07/07 11:37:47 (permalink)
0

How do I tell make not to make the hex file in the "Extra Loadables"

I added a hex file as an "Extra loadables" in the Project Properties dialog.  Now when I push the compile button the make the project it complains it doesn't know how to make the hex file I specified.
 
make[2]: *** No rule to make target 'C:/.../MD_Bootloader\(v0.7\).hex', needed by dist/Production/production/MD_Firmware_Rev_4.1.X.production.hex'. Stop.
make[2]: *** Waiting for unfinished jobs....
make[1]: *** [.build-conf] Error 2
make: *** [.build-impl] Error 2
 
 
How to I tell make it doesn't need to make the bootloader hex file?
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5