• AVR Freaks

Hot!RN2483 reset pin pulse

Author
parkerpics
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2020/06/09 01:29:54
  • Location: 0
  • Status: offline
2020/07/07 00:27:30 (permalink)
0

RN2483 reset pin pulse

Hi,
My understanding is that in order to reset the device using the reset pin an active low pulse should be introduced to the pin.
In my application i cut power to the module every so often for battery saving. What is the correct procedure for resetting the lora module?
Should i give an active low to the reset pin and then return it to its normal high state before cutting power?
Should i just give an active low to the reset pin before cutting power?
 
thanks
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5