• AVR Freaks

Hot!collect2.exe: error: ld returned 255 exit status

Author
you_sun
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2020/02/25 12:50:33
  • Location: 0
  • Status: offline
2020/07/03 21:39:23 (permalink)
0

collect2.exe: error: ld returned 255 exit status

Dear Microchip expert, 
I am an EE on the hardware side. have some experience on TI code composer studio. totally new to XIDE. 
I just redesigned an old board. with a firmware project compiled with MPLAB IDE v8.92. 
I following the suggestion to convert it to XIDE V5.40. I spent days to install the IDE, compiler, Harmony and googled to eliminate all conflict Errors. finally, I got this ld error, which I don't think I can figure out. 
attached is the output of the compile. 
need suggestion to compile this project, 
should I find an IDE V8.92? I think it may be easier, but I think Microchip recommends to use new tools. 
should I create a new project step by step, or just import the legacy project to the new XIDE?
 
Have a great and safe holiday,
 
David Sun
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5