• AVR Freaks

Hot![Harmony v3] Creating own Package

Author
mvollmer
Junior Member
  • Total Posts : 92
  • Reward points : 0
  • Joined: 2013/08/20 22:58:04
  • Location: Germany
  • Status: offline
2020/07/02 02:13:36 (permalink)
2 (1)

[Harmony v3] Creating own Package

Hi folks,
Is there any Documentation about creating own packages for harmony v3? Is there an example to start with? I would like to create my own package for a serial flash. I've already created some for harmony v2.

What i can see is that its needed to do some stuff in python now. Any experience with this?
 
Because Harmony v3 uses git, i hope its possible to maintain the own package code in a gitlab repo.
 
 

with kind regards
mvolllmer
 
PIC Experience with PIC24FJ256GB110 and PIC32MX3XX_4XX Family
#1

1 Reply Related Threads

    arpananand
    Super Member
    • Total Posts : 498
    • Reward points : 0
    • Joined: 2009/11/18 04:35:42
    • Location: 0
    • Status: offline
    Re: [Harmony v3] Creating own Package 2020/07/02 07:08:03 (permalink)
    0
    currently this is not documented.
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5