• AVR Freaks

Hot!Is there a way to place a library at a specific memory location?

Author
rangeck
New Member
  • Total Posts : 27
  • Reward points : 0
  • Joined: 2011/03/01 14:13:58
  • Location: 0
  • Status: offline
2020/07/01 06:41:23 (permalink)
0

Is there a way to place a library at a specific memory location?

With XC32, is there a way to place a library's program code at a specific flash memory location?
 
Using MPLAB X, I pull up the top level project properties and click libraries. I add my library projects, but don't see any options entry at all. 
#1

1 Reply Related Threads

    andersm
    Super Member
    • Total Posts : 2839
    • Reward points : 0
    • Joined: 2012/10/07 14:57:44
    • Location: 0
    • Status: offline
    Re: Is there a way to place a library at a specific memory location? 2020/07/01 07:06:22 (permalink)
    0
    Yes, with a custom linker script.
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5