• AVR Freaks

AnsweredHot!ATWINC1500 For (Extreme) Beginner

Page: < 12 Showing page 2 of 2
Author
IBrokeIt
Starting Member
  • Total Posts : 64
  • Reward points : 0
  • Joined: 2019/08/13 12:07:00
  • Location: 0
  • Status: offline
Re: ATWINC1500 For (Extreme) Beginner 2020/07/08 19:36:44 (permalink)
0
Hi KJSmeets,
 
I am significantly further behind than you are.  I just built up the 24 platform and got USB CDC driver configured.  I am working on porting the winc1500 driver set over.  I am using a 128GB202 so looks like the exact same form factor you have.  In going through all these files included with the MLA set it looks like there is a substantial amount of IO remapping that needs to be done.  Quite formidable task from looking at it imo.  How did you get started with this?  Did you use MCC to generate code or go through the MLA example and map everything over to the smaller form factor devices it looks like we are both using?  Looking through all the MLA includes like ugggh...this looks like a good time.
 
#21
Page: < 12 Showing page 2 of 2
Jump to:
© 2020 APG vNext Commercial Version 4.5